This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRA821U: After configuring Native Ethernet mode (eth1, eth2, eth3, eth4), is it possible to use 2 ports in MAC mode and 2 ports in switch mode?

Part Number: DRA821U


Tool/software:

Hi


I am reviewing the usage of Native Ethernet mode.

When configuring Native Ethernet mode on the EVM, four ports (eth1, eth2, eth3, eth4) are created.
In this setup, is it possible to use eth1 and eth2 in MAC mode while using eth3 and eth4 in switch mode?

Please confirm.

Regards,

Dohyeon.kim