Other Parts Discussed in Thread: SYSCONFIG,
Tool/software:
Hello,
I was able to configure successfully the SDRAM on our custom board with CCS 20.1.0, project-less debug session running AM62B-P1 EVM gel scripts. However, these scripts configure the 2GB space for 16Gb x 16 chip used on the EVM, while our board is using one single rank 32Gb x 16 DDR4 chip.
I tried replacing the AM62x-DDR4-1600MTs.gel (located in C:\ti\ccs2010\ccs\ccs_base\emulation\gel\AM62x\AM62_DDRSS\si_configs) with one generated by the SysConfig DDR4 configuration tool for our 32Gb x 16 chip but it is not working. Is there anything else that needs to be changed?
The 32Gb x 16 DDR4 SDRAM chips are actually two 16Gb x 8 dies in the package so that I wanted to try setting the gel scripts for two 16Gb x 8 chips but couldn't find where the number of chips are set.
Thanks,
Kris