Tool/software:
Hi
I want to check if RTOS SDK support SD boot on AM62L?
If yes, do we have any guide?
Thanks
Zekun
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Anil
Do you have feedback on this issue?
I am using Windows Host do to the UFU boot according to the guide, but it only consists of how to flash tiboot3 and app under Linux host, can you provide how to flash image in DFU boot with Windows?
When will the SDK guide get upgraded, seems it lacks much content.
Regards
Zekun
Hello Zekun,
There is no support for SD boot mode on the RTOS side.
Currently, we do support USB DFU loading, which means that the Application is loaded onto the DDR or MSRAM from a USB DFU tool.
We don't support DFU Flashing in RTOS side .
Regards,
Anil.