Other Parts Discussed in Thread: SK-AM62B
Tool/software:
Hello TI.
We are using yocto SDK 9.0
We face below display issue.
We built system image "tisdk-default-image" and put on SD Card to boot.
1. First boot, it looks normal which the default TI psplash boot logo/progress bar is shown on LCD.
We also can display our image on LCD using fbi cmd that we added in the image. (in this case, sometime weston & works, sometime not)
1_first_boot_log_splash_show.txt
2. After the first boot, we reboot our board, then nothing is shown on LCD.
- issue waston cmd failed 100%
- then sometime we can display our image on LCD by using fbi (in first part of log below), most we cannot.
2_second_boot_log_pspaslh_notshown.txt
May you help?
BR,
Paul