1462.temp9_x.rarthe program in "temp9_x.rar" is for the SPI data transfer
i copyed the code from the platform folder
if i use the POST BOOT mode power on the board open the ccs5.03 link blackhawk tool build the prog load
the four leds can work correctly and the spi nor flash can be read out.
but
if i use the NO BOOT mode power on the board open the ccs5.03 link blackhawk tool build the prog load
the four leds can not work correctly and the spi nor flash cannot be read out.
please help me