Part Number: AM623
Tool/software:
Hi Expert,
The customer is expected to use QPSI boot mode
Refer to the boot mode configure file for Bit8 lclk settings. Customer selects QSPI Flash without DQS signal, so it should be set to "0"
However, the document mentions that the LBCLKO signal will need to be used
Because EVB is an OSPI Flash with DQS, there is no special indication on how to use QSPI flash without DQS signal.
I would like to ask how to use this LBCLKO? Where should I pull this signal?



Thanks
Daniel