Dear TI,
what is the current state of Scalable Video Coding feature support for the H264 encoder OpenMAX component?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear TI,
what is the current state of Scalable Video Coding feature support for the H264 encoder OpenMAX component?
Hi Ivan,
What features of Scalable Video Coding is of interest to you?
Hi Venugopala,
I'm interested in options that can be set via IH264ENC_SVCCodingParams structure.
Also, is the IH264ENC_Profile::IH264SVC_HighProfile available in TI encoder component?
Using IH264ENC_SVCCodingParams structure of H264 Encoder component only Temporal Scalability can be achieved.
Then the OMX component should be available soon.
Answer is No.
Venugopala said:Then the OMX component should be available soon.
Do you mean the expected on the 9th of December 2011 "patch release", as stated here:
http://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/717/p/140602/509138.aspx#509138
?