Hi,
We work with the DM368 (Linux) and we want to build a specific configuration of PINMUX0. Indeed, we initially set YIN [7-0] as GPIO (8-bit parallel for transmit data) and a second time (on linux user space) as imager input. Is the DM368 supports the dynamic change of PINMUX0? Can we make this change from the linux user space?
In the case of the configuration as 8 bit parallel (GPIO), what could be the maximum frequency of data transmission?
One last question completely independent of the previous, what is the maximum frequency of the SPI module (transmission frequency) in master mode??
Thank you in advance.
Best regards
Sakho