This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Davinci DM357:Unable to mount root fs via NFS, trying floppy and Unable to get nfsd port number from server, using default



Hi All

i have installed ubuntu11,10 with ext4(filesystem is saported )

Please give help ............

I am planing to load the kernel & file system so i faced so many prob .......

PROB-1:

root@here3itech-desktop:/home/here3i-tech/workdir/filesys# /usr/sbin/exportfs -av
exportfs: /etc/exports [2]: Neither 'subtree_check' or 'no_subtree_check' specified for export "*:/home/here3i-tech/workdir/filesys".
  Assuming default behaviour ('no_subtree_check').
  NOTE: this default has changed since nfs-utils version 1.0.x

exportfs: scandir /etc/exports.d: No such file or directory

exporting *:/home/here3i-tech/workdir/filesys
exporting *:/nfsroot
root@here3itech-desktop:/home/here3i-tech/workdir/filesys# /sbin/service nfs restart
bash: /sbin/service: No such file or directory
root@here3itech-desktop:/home/here3i-tech/workdir/filesys#

PROB-2:

while booting .....................

IP-Config: Complete:                                                                                                                                                                                        
      device=eth0, addr=192.168.0.54, mask=255.255.255.0, gw=192.168.0.2,                                                                                                                                   
     host=192.168.0.54, domain=3i-corporation.co.in, nis-domain=(none),                                                                                                                                     
     bootserver=0.0.0.0, rootserver=0.0.0.0, rootpath=                                                                                                                                                      
Looking up port of RPC 100003/2 on 0.0.0.0                                                                                                                                                                  
portmap: server 0.0.0.0 not responding, timed out 
                                                                                                                                                          
Root-NFS: Unable to get nfsd port number from server, using default                                                                                                                                         
Looking up port of RPC 100005/1 on 0.0.0.0                                                                                                                                                                  
portmap: server 0.0.0.0 not responding, timed out                                                                                                                                                           
Root-NFS: Unable to get mountd port number from server, using default                                                                                                                                       
mount: server 0.0.0.0 not responding, timed out                                                                                                                                                             
Root-NFS: Server returned error -5 while mounting /tftpbootnfshost)rootpath)                                                                                                                                
VFS: Unable to mount root fs via NFS, trying floppy.                                                                                                                                                        
VFS: Cannot open root device "nfs" or unknown-block(2,0
)                                                                                                                                                    
Please append a correct "root=" boot option                                                                                                                                                                 
Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(2,0)

so please help me...... then i'll go for the next step