I want to use the Sys_clkreq.
I saw Table 4-27 of SPRUGR0B.
I understood that Output buffer conditions of the Sys_clkreq is controlled by the Internal Clock request.
Is there the information to control the Internal Clock request?
The Internal Clock request is seen in Figure 4-42.
In addition, it is seen in Table 4-29.
Are all these the same things?
In Figure 4-42, the Internal clock request is output by the Device power FSM.
What is the Device power FSM?
Thank you.