Hello,
Here I am facing on problem.
We are using Custom board for our application. I have placed U boot as well as QNX image on SPI flash.
But some times, QNX image fails to boot or crashes. I suppose there is problem with SPI, Because the same Image booted properly from NAND.
here I could not figure out the problem.
When I issue
> sf probe <>
> sf read <> <> <>
> sleep 5
> go <>
it is working fine...!
But when i automate the scripts
eg: bootcmd ' sf probe<>; sf read <> <> <>; sleep 5; go <>'
I could not able to load the image...
What could be the problem..
When I type one cmd at a time on u boot to boot from SPI it is working ffine..
but when i automate it is not working.
I am getting error as
## starting application at 0xc0008000
Please help me in this regard.
I used AIS gen tool to generate SPI Uboot bin with SPI Clock of 20MHz
My QNX oS image size is around 3.28 MB.