This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6670 VCP2 test example

Hello,

   I am planning to use C6670' VCP2 . But i can't  find  any  VCP2 test example in the MCSDK 2.0.x .

Is there an example VCP2 project for C6670 to test  VCP2  conveniently ?

 Thanks. 

  • hello Fei,

    Please find the VCP2 BER example project @

    https://gforge.ti.com/gf/download/user/9358/5869/BER.zip

    Let me know if you can access it.

    Regards,

    Kishore.

  • Hello,

    I ran this example code and found BER results according to 12.2K NB-AMR  - class A (frame lenght = 103, rate = 2, k = 9 ...) as below. Are these results correct and what is the main purpose of using sigma in ' void AddAWGN_fixpt ' function?

    VCP2 test Sigma=0.90000 BER : 2.638927e-02 VCP2 Hardware BER: 2.638927e-02 ;

    VCP2 test Sigma=0.85000 BER : 7.446508e-03 VCP2 Hardware BER: 7.446508e-03 ;
    VCP2 test Sigma=0.80000 BER : 2.789065e-03 VCP2 Hardware BER: 2.789065e-03 ;
    VCP2 test Sigma=0.75000 BER : 3.489906e-04 VCP2 Hardware BER: 3.489906e-04 ;

    Thanks

    Anil

  • Hello,

      I have downloaded the project under https://gforge.ti.com/gf/download/user/9358/5869/BER.zip.

    Unable to build the project. 

    Project log is attached in this mail. Please have a look.


    Regards

    Rajendra Hegde

    !CONFIGURATION: 'com.ti.ccstudio.buildDefinitions.C6000.Debug.1149743120' [Wed Oct 09 17:12:15 IST 2013]
    
    	!TOOL: 'com.ti.ccstudio.buildDefinitions.C6000_7.4.exe.compilerDebug.1272471992'
    
    		!WARNING: Unresolved option: com.ti.ccstudio.buildDefinitions.C6000_7.3.compilerID.SILICON_VERSION
    
    		!WARNING: Unresolved option: com.ti.ccstudio.buildDefinitions.C6000_7.3.compilerID.DEBUGGING_MODEL
    
    		!WARNING: Unresolved option: com.ti.ccstudio.buildDefinitions.C6000_7.3.compilerID.OPT_LEVEL
    
    		!WARNING: Unresolved option: com.ti.ccstudio.buildDefinitions.C6000_7.3.compilerID.INCLUDE_PATH
    
    		!WARNING: Unresolved option: com.ti.ccstudio.buildDefinitions.C6000_7.3.compilerID.DISPLAY_ERROR_NUMBER
    
    		!WARNING: Unresolved option: com.ti.ccstudio.buildDefinitions.C6000_7.3.compilerID.DIAG_WARNING
    
    		!WARNING: Unresolved option: com.ti.ccstudio.buildDefinitions.C6000_7.3.compilerID.ABI
    
    	!TOOL: 'com.ti.ccstudio.buildDefinitions.C6000_7.4.exe.linkerDebug.2007043598'
    
    		!WARNING: Unresolved option: com.ti.ccstudio.buildDefinitions.C6000_7.3.linkerID.OUTPUT_FILE
    
    		!WARNING: Unresolved option: com.ti.ccstudio.buildDefinitions.C6000_7.3.linkerID.MAP_FILE
    
    		!WARNING: Unresolved option: com.ti.ccstudio.buildDefinitions.C6000_7.3.linkerID.STACK_SIZE
    
    		!WARNING: Unresolved option: com.ti.ccstudio.buildDefinitions.C6000_7.3.linkerID.HEAP_SIZE
    
    		!WARNING: Unresolved option: com.ti.ccstudio.buildDefinitions.C6000_7.3.linkerID.generatedLinkerCommandFiles
    
    		!WARNING: Unresolved option: com.ti.ccstudio.buildDefinitions.C6000_7.3.linkerID.LIBRARY
    
    		!WARNING: Unresolved option: com.ti.ccstudio.buildDefinitions.C6000_7.3.linkerID.SEARCH_PATH
    
    		!WARNING: Unresolved option: com.ti.ccstudio.buildDefinitions.C6000_7.3.linkerID.ABSOLUTE_EXE
    
    
    !CONFIGURATION: 'com.ti.ccstudio.buildDefinitions.C6000.Debug.1149743120' [Wed Oct 09 17:14:23 IST 2013]
    
    	!TOOL: 'com.ti.ccstudio.buildDefinitions.C6000_7.4.exe.compilerDebug.890880620'
    
    		!WARNING: Unresolved option: com.ti.ccstudio.buildDefinitions.C6000_7.3.compilerID.SILICON_VERSION
    
    		!WARNING: Unresolved option: com.ti.ccstudio.buildDefinitions.C6000_7.3.compilerID.ABI
    
    	!TOOL: 'com.ti.ccstudio.buildDefinitions.C6000_7.4.exe.linkerDebug.1502090176'
    
    		!WARNING: Unresolved option: com.ti.ccstudio.buildDefinitions.C6000_7.3.linkerID.OUTPUT_FILE
    
    		!WARNING: Unresolved option: com.ti.ccstudio.buildDefinitions.C6000_7.3.linkerID.LIBRARY
    
    
    !CONFIGURATION: 'com.ti.ccstudio.buildDefinitions.C6000.Debug.1149743120' [Wed Oct 09 17:15:53 IST 2013]
    
    	!TOOL: 'com.ti.ccstudio.buildDefinitions.C6000_7.4.exe.compilerDebug.475651367'
    
    		!WARNING: Unresolved option: com.ti.ccstudio.buildDefinitions.C6000_7.3.compilerID.SILICON_VERSION
    
    		!WARNING: Unresolved option: com.ti.ccstudio.buildDefinitions.C6000_7.3.compilerID.ABI
    
    	!TOOL: 'com.ti.ccstudio.buildDefinitions.C6000_7.4.exe.linkerDebug.1009153397'
    
    		!WARNING: Unresolved option: com.ti.ccstudio.buildDefinitions.C6000_7.3.linkerID.OUTPUT_FILE
    
    		!WARNING: Unresolved option: com.ti.ccstudio.buildDefinitions.C6000_7.3.linkerID.LIBRARY