This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Are there some test examples for C6670 CSL?

hello,

I find  C6678 have  all CSL  test examples ,but C6670 only AIF have a  C6670 CSL  test examples  in the MCSDK.

Are there some test examples  for  C6670 CSL?

 

thanks

  • Hi,

    Actually the most of modules of C6678 and C6670 are the same, except for the number of Cores and C6670 has more accelerators than C6678.

    So if you want to make use of the common modules of the two chips(such as EDMA,XMC etc.) ,the examples of C6678 are applicable.

     

    Allen

  • Hello,

       I am planning to use C6670' VCP2 . But i can't  find  any  VCP2 test example in the MCSDK 2.0.x .

    Is there an example VCP2 project for C6670 to test  VCP2  conveniently ?

     Thanks.