This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM816X EZSDK 5011 OMX encoder DEMO. 2 channel 1080p60 encoding problem.



I have a issue in OMX demo EZSDK 5011.

I want encode 2 1080p60 H.264 on Two different VICP. the result shows that the  framerate is not up to 60. the time assumption of encoding is 20ms/perframe...

 if I encode one 1080p60, the framerate is ok.

The time assumption is 14ms/perframe .....

How can I encoder 2 channel independently? Anybody has encountered the same problem?