Part Number: AM620-Q1
Tool/software:
Hi, Dear Expert
When AM62 in FFI w/ reset isolation, does it support "internal" SPI or I2C connection?
Thank You.
Gibbs
Reference,

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: AM620-Q1
Tool/software:
Hi, Dear Expert
When AM62 in FFI w/ reset isolation, does it support "internal" SPI or I2C connection?
Thank You.
Gibbs
Reference,

"internal" SPI or I2C connection?
I need more context on the meaning of the word internal here.
Could you elaborate more on what is the use case, apart from whats highlighted in one of the responses.
Regards,
Vaibhav
Hi, Vaibhav
Thanks you replies.
The word, "internal SPI or I2C connection" means "internal" SPI/I2C connection (interface) between main domain and mcu domain in SOC.
Basically, this interface do not have "physical pin out" on chip.
for example, one SPI interface in MCU domain, and another SPI interface in main domain, this SPI interface connection each other inside chip, but they do not have physical pin out.
Once FFI or MCU isolation enabled, RPMsg could be prohibited, so "internal SPI or I2C connection" is the only way to bridge communication between these two domain.
Thanks
Gibbs
Hi,
Thanks for your patience.
Basically, this interface do not have "physical pin out" on chip.
for example, one SPI interface in MCU domain, and another SPI interface in main domain, this SPI interface connection each other inside chip, but they do not have physical pin out.
Can you please specify the exact pins which you are asking about/looking at?
I am also assuming you are talking with respect to custom board?
Regards,
Vaibhav
Hi, Vaibhav
Pls reference TDA4 TRM (Ver C), this function what's I want to know on AM62.
p114


Thank You.
Gibbs
Hi,
I have gone through the AM62x TRM and I have not found anything as such which you have highlighted above from MCSPI section.
I have not seen anything as such for MCSPI at the moment based off TRM and datasheet as well. I have also looked at the block diagram but I see no internal connections for MCSPI.
Regards,
Vaibhav
Hi, Vaibhav
I think it should be not support.
so it should be connect SPI between main/mcu domain by physical pin out.
Thanks
Gibbs