This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Why the pins GP1_IO31 and GP1_IO30 are unconnected

In the netra evm schematics Page 14(JTAG/GPIO/RESET), Why the pins GP1_IO31 and GP1_IO30 are unconnected.

Ref:http://support.spectrumdigital.com/boards/evm816x/reve/

  • Hello,

    The device pins J32 and J33 are connected, they are just connected through the alias names "ENET_INTn" and "MSP430_INT" instead of through the names "GP1_IO31" and "GP1_IO30".  The tool treats both port aliases as if they are the same port.

    Regards,
    Marc