Part Number: SK-AM62P-LP
Tool/software:
Hello TI,
I am using the SK-AM62P-LP EVM and running Debian Trixie OS (version 10.00.00) along with the MCU+ SDK.
After reading the TRM, I have understood the functionality of the ECC (Error Correction Code) module. For functional safety, we would like to enable ECC for DDR4, and I have a few questions regarding this:
-
DDR4 ECC is not enabled by default. Since we require it, we plan to enable it in the U-Boot configuration, rebuild it, and deploy it to the system. Could you please guide us through the procedure? Specifically, which flags or device tree nodes need to be changed to enable DDR4 ECC?
-
We are initializing ECC for MCU_MSRAM (512 KB, with two endpoints: 8 and 21, each 256 KB), which are accessed through the MAIN_ECC_AGGR0 and processed by the R5 core.
If we enable ECC for DDRSS, can both DDR ECC and MCU_MSRAM ECC run simultaneously without conflict?
Thank you,
RajKumar