HI,
I have c5515 ezdsp USB kit. there is nor flash on the board itself to make the board stand alone.
i want to use SPI EEPROM as external memory for burning the code inside.
i downloaded the c5505 programmer code from the code.google.com .
i also made the connection from c5515 ezdsp borad to SPI EEPROM as exactly shown in c5515 evm borad.
but still when i try to burn the code it shows write failed error.
Please suggest.
if any Programmer for SPI eeprom on C5515 ezdsp board.available pls share it.