This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM6411: MMC/SDIO drivers rise/fall timing and slew rates

Part Number: AM6411

Tool/software:

Dear Sitara HW champs,

Could you provide ASAP the rise/fall times and slew rates of drivers (IO cells) of MMC1 (SDIO) at 3V3 and 1V8 in different modes (specially default mode at <25MHz)?

Thank you!

Best regards,

Guillaume

  • We do not define output rise/fall times because these parameters depend on the actual system implementation. You will need to use the IBIS model for the respective AM64x pin and simulate the rise/fall times based on your actual PCB load.

    Regards,
    Paul