This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM4378: The number of MAC address

Part Number: AM4378


Tool/software:

Hi AM4378 Champ !

I would like to inquire about how many MAC addresses are assigned to the AM4378BZDND100.

Thanks.

Regards, Jack

  • Hi,

    The TRM describes in table Table 7-11 there are two MAC addresses programmed into these registers:

    630h CTRL_MAC_ID0_LO Section 7.3.1.26

    634h CTRL_MAC_ID0_HI Section 7.3.1.27

    638h CTRL_MAC_ID1_LO Section 7.3.1.28

    63Ch CTRL_MAC_ID1_HI Section 7.3.1.29

    These MAC addresses are one that TI has purchased, typically customers prefer to purchase their MAC IDs.

    Best Regards,

    Schuyler