This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM62A7-Q1: Power consuption on VDDSHV of AM62Ax

Part Number: AM62A7-Q1


Tool/software:

Hi,

I am using Power estimator tool for AM62Ax for my application. I am tryin to figure out the current consumptions on VDDSHVx rails. Looking at the estimator sheet, I couldn't understand the current for each  VDDSHVx rails. As it has below supply rails only. Does it auto calculates total current of SOC_DVDD1V8 and SOC_DVDD3V3 with respect to IO selection in the same sheet? 

Sharing below images of power estimation tool for reference.

Thanks,

Nikunj

  • Hi Nikunj,

    The IOs power consumption is calculated based on the LVCMOS IO/Peripherals mode config, utilization% and the fixed 1.8V or 3.3V rails that are not shown in the summary sheet. An example of a fixed 3.3V rail is VDDA_3P3_USB. 

    Thanks,

    Brenda