This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA3MV: DDR3 related fault issue

Part Number: TDA3MV


Tool/software:

Hi Team,

My customer has some issue while they are using TDA3MVRBFABFRQ1

with 2pcs DDR3(K4B4G1646E-BNCB)

Here's the log they get.

What can be the cause of this problem?

if you need more data to analyze this please let me know.

Regards,

Ted

  • Hi,

    Is this a new design, or existing design? 

    How many boards have been built / tested, and how many show the issue?

    Does the failure occur every boot cycle, or just sometimes? 

    Regards,
    Kevin

  • The board is on the validation state.

    they built 300boards, and 5 board has an issue.

    once the issue happens, it happens every boot cycle.

    Regards,

    Ted

  • Hi Kevin,

    Can you take a look at this?

    Regards,

    Ted

  • Hi,

    Do you have the register settings they are using , specifically the array they are using to setup the PHY registers? (example below)

    Regards,
    Kevin

    const unsigned int DRA75x_DDR3L_532MHz_TI_EVM_revH_emif1_ext_phy_regs [] = {
        0x04040100,
        0x006B006B,
        0x006B006B,
        0x006B006B,
        0x006B006B,
        0x006B006B,
        0x00320032,
        0x00320032,
        0x00320032,
        0x00320032,
        0x00320032,
        0x00600060,
        0x00600060,
        0x00600060,
        0x00600060,
        0x00600060,
        0x00400040,
        0x00400040,
        0x00400040,
        0x00400040,
        0x00400040,
        0x00800080,
        0x00800080,
        0x40010080,
        0x08102040,
        0x00000000,
        0x00000000,
        0x00000000,
        0x00000000,
        0x00000000,
        0x00000000,
        0x00000000,
        0x00000000,
        0x00000000,
        0x00000000,
        0x00000077
    };
  •     SDRAM_TIM_1 = 0xCEEF266BU;
        SDRAM_TIM_2 = 0x30BF7FDAU;
        SDRAM_TIM_3 = 0x407F8BA8U;
    
        SDRAM_REF_CTRL = 0x00001035U;
        SDRAM_REF_CTRL_INIT = 0x000040F1U;
        SDRAM_CONFIG = 0x61851BB2U;
    
        EMIF_PHY_READ_LATENCY = 0xEU;
        EMIF_PHY_INVERT_CLKOUT = 0x1U;
        EMIF_PHY_HALF_DELAY_MODE = 0x1U;
        EMIF_PHY_DQ_OFFSET = 0x40U;
        EMIF_PHY_CTRL_SLAVE_RATIO = 0x80U;
    
        DISABLE_READ_LEVELING = 0x1U;
        DISABLE_READ_GATE_LEVELING = 0x1U;
        DISABLE_WRITE_LEVELING = 0x1U;
    
        /* EXT_PHY_CTRL_xx are used only in case of  HW_LEVELING_ENABLED  =  0*/
        /* EMIF_PHY_FIFO_WE_SLAVE_RATIO (RD_DQS_GATE) */
        EXT_PHY_CTRL_2 = 0x07000075U;
        EXT_PHY_CTRL_3 = 0x0700007AU;
        EXT_PHY_CTRL_4 = 0x07000076U;
        EXT_PHY_CTRL_5 = 0x07000078U;
        EXT_PHY_CTRL_6 = 0x07000700U;
    
        /* EMIF_PHY_RD_DQS_SLAVE_RATIO */
        EXT_PHY_CTRL_7 = 0x0000003BU;
        EXT_PHY_CTRL_8 = 0x0000003BU;
        EXT_PHY_CTRL_9 = 0x00000040U;
        EXT_PHY_CTRL_10 = 0x0000003BU;
        EXT_PHY_CTRL_11 = 0x00000000U;
    
        EXT_PHY_CTRL_12 = 0x01A3005DU;
        EXT_PHY_CTRL_13 = 0x00E0005FU;
        EXT_PHY_CTRL_14 = 0x03160061U;
        EXT_PHY_CTRL_15 = 0x005E0066U;
        EXT_PHY_CTRL_16 = 0x02320130U;
    
        /* EMIF_PHY_WR_DQS_SLAVE_RATIO */
        EXT_PHY_CTRL_17 = 0x018B00045U;
        EXT_PHY_CTRL_18 = 0x00C80047U;
        EXT_PHY_CTRL_19 = 0x02FE0049U;
        EXT_PHY_CTRL_20 = 0x0046004EU;
        EXT_PHY_CTRL_21 = 0x02320130U;		

    Here's their register setting. When they did device swap and then on both board it worked well, so they stopped the investigation.

    Assumption : SMT issue

    Regards,

    Ted