Part Number: AM625
Other Parts Discussed in Thread: SK-AM62-LP
Tool/software:
We have a custom board using the AM6232, the Ethernet Phys are Micrel XZ8041 in RMII mode.
I have created the 3 files needed files from ti-u-boot-2024.04 and copied them to my DHCP/TFP server which is connected to the AM62 via a USB Ethernet port i.e. a dedicated port.
On power up I can see the initial TFTP for tiboot.bin work and the SPL executes.
Despite seeing the Phy being detected and the link being valid I do not see any tx output for the BOOTP broadcast.
Are there some areas you could suggest for me to look at to try and diagnose why the tx is not making it to the Ethernet output ?
Boot log is attached.
Thank you.
U-Boot SPL 2024.04-00002-gbaa288e477f-dirty (Mar 27 2025 - 09:38:30 +0000)SYSFW ABI: 4.0 (firmware rev 0x000a '10.0.8--v10.00.08 (Fiery Fox)')SPL initial stack usage: 13392 bytesTrying to boot from eth deviceethernet@8000000port@1 connected to Micrel KSZ804 mode rmiieth0: ethernet@8000000port@1ethernet@8000000port@1 Waiting for PHY auto negotiation to complete..... donelink up on port 1, speed 100, full duplexBOOTP broadcast 1BOOTP broadcast 2BOOTP broadcast 3BOOTP broadcast 4BOOTP broadcast 5BOOTP broadcast 6BOOTP broadcast 7BOOTP broadcast 8BOOTP broadcast 9BOOTP broadcast 10BOOTP broadcast 11BOOTP broadcast 12BOOTP broadcast 13BOOTP broadcast 14BOOTP broadcast 15BOOTP broadcast 16BOOTP broadcast 17
Retry time exceeded; starting againudma_stop_mem2dev: peer not stopped TIMEOUT !Problem booting with BOOTPSPL: failed to boot from all boot devices### ERROR ### Please RESET the board ###