Tool/software:
In the `ti-processor-sdk-rtos-j721e-evm-10_01_00_04/vision_apps/apps/basic_demos/app_dof/main.c`, I found that the output from `vxGaussianPyramidNode` is assigned to `obj->pyramidObj.pyr_ref`, as follow snippet.
status = app_create_graph_pyramid(obj->graph, &obj->pyramidObj, obj->pyramidObj.input_img[0], obj->pyramidObj.pyr_ref );
And, `obj->pyramidObj.pyr_ref` is the index -1 of the `pyramidObj->pyr_delay` delay object, as follow snippet of `ti-processor-sdk-rtos-j721e-evm-10_01_00_04/vision_apps/apps/basic_demos/app_dof/dof_pyramid_module.c`.
pyramidObj->pyr_delay = vxCreateDelay(context, (vx_reference)pyr_exemplar, 2); APP_ASSERT_VALID_REF(pyramidObj->pyr_delay); pyramidObj->pyr_ref = (vx_pyramid)vxGetReferenceFromDelay(pyramidObj->pyr_delay, -1); APP_ASSERT_VALID_REF(pyramidObj->pyr_ref); vxSetReferenceName((vx_reference)pyramidObj->pyr_ref, "PyramidReference"); pyramidObj->pyr_cur = (vx_pyramid)vxGetReferenceFromDelay(pyramidObj->pyr_delay, 0); APP_ASSERT_VALID_REF(pyramidObj->pyr_cur); vxSetReferenceName((vx_reference)pyramidObj->pyr_cur, "PyramidCurrent");
If I don't misunderstand, index -1 is of the delay object is the previous frame, and index 0 of the delay object is the current frame (i.e., `pyramidObj->pyr_cur`).
And, indeed, the `obj->pyramidObj.pyr_cur` and `obj->pyramidObj.pyr_ref` are respectively assigned to the arguments `input_current` and `input_reference` of the `tivxDmpacDofNode`, as follow snippet of `ti-processor-sdk-rtos-j721e-evm-10_01_00_04/vision_apps/apps/basic_demos/app_dof/main.c`.
status = app_create_graph_dofproc(obj->graph,
&obj->dofprocObj,
obj->dofprocObj.dof_config,
obj->pyramidObj.pyr_cur,
obj->pyramidObj.pyr_ref,
obj->dofprocObj.flow_vector_field_in,
obj->dofprocObj.flow_vector_field_out );
So my question is: Why is the latest output from `vxGaussianPyramidNode` assigned to `obj->pyramidObj.pyr_ref` (i.e., the previous frame) instead of `obj->pyramidObj.pyr_cur` (i.e., the current frame)? Is this a bug? But the resulting output images seem correct.