Part Number: TDA4VM
Tool/software:
Hello
I'm using RPOC078A and 79A using TDA4VM EV-KIT.
Currently, there is an intermittent phenomenon that the product cannot be booted, so I'm inquiring.
The power input to VCCA_3V3(U27-4PIN), which is PMIC input, is confirmed to be normal,
I'm using RPOC078A and 79A using TDA4VM EV-KIT.
Currently, there is an intermittent phenomenon that the product cannot be booted, so I'm inquiring.
The power input to VCCA_3V3(U27-4PIN), which is PMIC input, is confirmed to be normal,
but I am inquiring because the power output of PMIC is not working.(1.8V, 0.8V Just 0V)
When this phenomenon occurs, it consumes about 900 mA, which consumes about 500 mA, and it is believed that low-frequency sound is generated on the board.
When this phenomenon occurs, it consumes about 900 mA, which consumes about 500 mA, and it is believed that low-frequency sound is generated on the board.
nPWRON/ENABLE input Vol: 3.3V
Please check.
Thank you.