This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Need Help to resolve Booting Issues on EZSDK 5.03

Hi there,

I noticed that ezsdk5.03 is not backward compatible as the boot loader is concerned. so I created a new boot SD
card by following <<PSP U-boot>>(page 20) documentation. But things didn't quite work out. Could someone
shed some light on this?

Thanks a lot.

-Perry

Q1. I assume the SD boot would be the simplest booting scenario. But even with SD boot, I found that the driver
loading failed. I quote my environment variables that embedded in boot.scr file as following:

setenv bootargs 'console=ttyO2,115200n8 rootdelay=5 root=/dev/mmcblk0p2 rw mem=384M earlyprink vram=50M ti816xfb.vram=0:16M,1:16M,2:6M ip=off noinitrd'
setenv bootcmd 'mmc rescan 0; fatload mmc 0 0x81000000 uImage; bootm 0x81000000'
boot


Q2. I normally prefer to using NFS to work on the DM8168 evm. This is the first release that I had trouble to set it up.
I cannot use "saveenv" to save the boot environment variable to NAND flash. I am sure that I was using the file boot.bin
that was built exactly built for NAND flash. I am also pretty sure the hardware switch (SW4) was set correctly. It have worked for
me for all previous releases.

Q3. I thought I was still able to mount the root file system through NFS without using the NAND flash by changing the
boot.scr file on SD card. But so far I have no luck. The tftpboot worked, but mounting file system failed.
I quote my setting in boot.scr (without the binary header) and console output as following.

setenv bootdelay '4'
setenv script_addr '0x80900000'
setenv autoload 'no'

setenv ethact 'DaVinci EMAC'
setenv ethaddr '90:d7:eb:1e:bc:b0'

setenv serverip '192.168.20.43'
setenv ipaddr '192.168.20.24'
setenv loadaddr '0x81000000'
setenv bootfile 'uImage-sdk11-2011-ddr3.bin'
setenv bootcmd 'tftpboot; bootm'
setenv bootargs 'console=ttyO2,115200n8 rootdelay=5 rw mem=384M earlyprintk notifyk.vpssm3_sva=0xBF900000
vram=50M ti816xfb.vram=0:16M,1:16M,2:6M root=/dev/nfs nfsroot=192.168.20.43:/home/perry/targetfs11 ip=dhcp'
----------------------------------------------------------------------------------------------


console output starts here.

-----------------------------------------------------------------------------------------------
U-Boot 2010.06 (Nov 10 2011 - 19:25:12)

DRAM: 2 GiB
Using default environment

MMC: OMAP SD/MMC: 0
Hit any key to stop autoboot: 0
raise: Signal # 8 caught
reading u-boot.bin

184792 bytes read
## Starting application at 0x80800000 ...


U-Boot 2010.06 (Nov 10 2011 - 18:55:59)

TI8168-GP rev 1.1

ARM clk: 987MHz
DDR clk: 796MHz

I2C: ready
DRAM: 2 GiB
NAND: HW ECC Hamming Code selected
NAND device: Manufacturer ID: 0x2c, Chip ID: 0xca (Micron NAND 256MiB 3,3V 16-bit)
NAND bus width 8 instead 16 bit
No NAND device found!!!
0 MiB
*** Warning - bad CRC or NAND, using default environment

MMC: OMAP SD/MMC: 0
Net: <ethaddr> not set. Reading from E-fuse
Detected MACID:90:d7:eb:1e:bc:b0
Ethernet PHY: GENERIC @ 0x01
DaVinci EMAC
Hit any key to stop autoboot: 0
raise: Signal # 8 caught
reading boot.scr

311 bytes read
Running bootscript from MMC/SD to set the ENV...
## Executing script at 80900000
raise: Signal # 8 caught
raise: Signal # 8 caught
reading uImage

2427768 bytes read
## Booting kernel from Legacy Image at 81000000 ...
Image Name: Arago/2.6.37-psp04.00.01.13/dm81
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 2427704 Bytes = 2.3 MiB
Load Address: 80008000
Entry Point: 80008000
Verifying Checksum ... OK
Loading Kernel Image ... OK
OK

Starting kernel ...

Uncompressing Linux... done, booting the kernel.
Linux version 2.6.37 (x0029463@swubn01) (gcc version 4.3.3 (Sourcery G++ Lite 2009q1-203) ) #1 Thu Nov 10 18:4
4:30 IST 2011
CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c53c7f
CPU: VIPT nonaliasing data cache, VIPT aliasing instruction cache
Machine: ti8168evm
vram size = 52428800 at 0x0
reserved size = 52428800 at 0x0
FB: Reserving 52428800 bytes SDRAM for VRAM
Memory policy: ECC disabled, Data cache writeback
OMAP chip is TI8168 1.1
Built 1 zonelists in Zone order, mobility grouping on. Total pages: 84736
Kernel command line: console=ttyO2,115200n8 rootdelay=5 root=/dev/mmcblk0p2 rw mem=384M earlyprink vram=50M ti
816xfb.vram=0:16M,1:16M,2:6M ip=off noinitrd
PID hash table entries: 2048 (order: 1, 8192 bytes)
Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)
Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)
Memory: 334MB = 334MB total
Memory: 333268k/333268k available, 59948k reserved, 0K highmem
Virtual kernel memory layout:
vector : 0xffff0000 - 0xffff1000 ( 4 kB)
fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
DMA : 0xffc00000 - 0xffe00000 ( 2 MB)
vmalloc : 0xd8800000 - 0xf8000000 ( 504 MB)
lowmem : 0xc0000000 - 0xd8000000 ( 384 MB)
pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB)
modules : 0xbf000000 - 0xbfe00000 ( 14 MB)
.init : 0xc0008000 - 0xc003a000 ( 200 kB)
.text : 0xc003a000 - 0xc049c000 (4488 kB)
.data : 0xc049c000 - 0xc04e3400 ( 285 kB)
SLUB: Genslabs=11, HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
NR_IRQS:407
IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts
Total of 128 interrupts on 1 active controller
GPMC revision 6.0
Trying to install interrupt handler for IRQ400
Trying to install interrupt handler for IRQ401
Trying to install interrupt handler for IRQ402
Trying to install interrupt handler for IRQ403
Trying to install interrupt handler for IRQ404
Trying to install interrupt handler for IRQ405
Trying to install interrupt handler for IRQ406
Trying to install type control for IRQ407
Trying to set irq flags for IRQ407
OMAP clockevent source: GPTIMER1 at 27000000 Hz
Console: colour dummy device 80x30
Calibrating delay loop... 986.31 BogoMIPS (lpj=4931584)
pid_max: default: 32768 minimum: 301
Security Framework initialized
Mount-cache hash table entries: 512
CPU: Testing write buffer coherency: ok
devtmpfs: initialized
omap_voltage_early_init: voltage driver support not added
regulator: core version 0.5
regulator: dummy:
NET: Registered protocol family 16
OMAP GPIO hardware version 0.1
OMAP GPIO hardware version 0.1
omap_mux_init: Add partition: #1: core, flags: 0
_omap_mux_get_by_name: Could not find signal i2c2_scl.i2c2_scl
_omap_mux_get_by_name: Could not find signal i2c2_sda.i2c2_sda
NOR: Can't request GPMC CS
registered ti816x_vpss device
registered ti816x_gpio_vr device
registered TI816x on-chip HDMI device
registered ti816x_sr device
registered ti81xx_vidout device
pm_dbg_init: only OMAP3 supported
Registered ti81xx_fb device
ti81xx_pcie: Invoking PCI BIOS...
ti81xx_pcie: Setting up Host Controller...
ti81xx_pcie: Register base mapped @0xd8820000
ti81xx_pcie: Starting PCI scan...
PCI: bus0: Fast back to back transfers enabled
bio: create slab <bio-0> at 0
regulator: VFB: 800 <--> 1025 mV at 1010 mV
vgaarb: loaded
SCSI subsystem initialized
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
registerd cppi-dma Intr @ IRQ 17
Cppi41 Init Done
omap_i2c omap_i2c.1: bus 1 rev4.0 at 100 kHz
omap_i2c omap_i2c.2: bus 2 rev4.0 at 100 kHz
Advanced Linux Sound Architecture Driver Version 1.0.23.
Switching to clocksource gp timer
musb-hdrc: version 6.0, host, debug=0
musb-hdrc musb-hdrc.0: dma type: dma-cppi41
musb-hdrc: kernel must blacklist external hubs
musb-hdrc musb-hdrc.0: MUSB HDRC host driver
musb-hdrc musb-hdrc.0: new USB bus registered, assigned bus number 1
usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
usb usb1: Product: MUSB HDRC host driver
usb usb1: Manufacturer: Linux 2.6.37 musb-hcd
usb usb1: SerialNumber: musb-hdrc.0
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
musb-hdrc musb-hdrc.0: USB Host mode controller at d881e000 using DMA, IRQ 18
musb-hdrc musb-hdrc.1: dma type: dma-cppi41
musb-hdrc: kernel must blacklist external hubs
musb-hdrc musb-hdrc.1: MUSB HDRC host driver
musb-hdrc musb-hdrc.1: new USB bus registered, assigned bus number 2
usb usb2: New USB device found, idVendor=1d6b, idProduct=0002
usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1
usb usb2: Product: MUSB HDRC host driver
usb usb2: Manufacturer: Linux 2.6.37 musb-hcd
usb usb2: SerialNumber: musb-hdrc.1
hub 2-0:1.0: USB hub found
hub 2-0:1.0: 1 port detected
musb-hdrc musb-hdrc.1: USB Host mode controller at d8826800 using DMA, IRQ 19
NET: Registered protocol family 2
IP route cache hash table entries: 4096 (order: 2, 16384 bytes)
TCP established hash table entries: 16384 (order: 5, 131072 bytes)
TCP bind hash table entries: 16384 (order: 4, 65536 bytes)
TCP: Hash tables configured (established 16384 bind 16384)
TCP reno registered
UDP hash table entries: 256 (order: 0, 4096 bytes)
UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
NET: Registered protocol family 1
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
RPC: Registered tcp NFSv4.1 backchannel transport module.
NetWinder Floating Point Emulator V0.97 (double precision)
PMU: registered new PMU device of type 0
omap-iommu omap-iommu.0: ducati registered
omap-iommu omap-iommu.1: sys registered
JFFS2 version 2.2. (NAND) ?? 2001-2006 Red Hat, Inc.
msgmni has been set to 650
io scheduler noop registered
io scheduler deadline registered
io scheduler cfq registered (default)
Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
omap_uart.0: ttyO0 at MMIO 0x48020000 (irq = 72) is a OMAP UART0
omap_uart.1: ttyO1 at MMIO 0x48022000 (irq = 73) is a OMAP UART1
omap_uart.2: ttyO2 at MMIO 0x48024000 (irq = 74) is a OMAP UART2
console [ttyO2] enabled
brd: module loaded
loop: module loaded
ahci ahci.0: forcing PORTS_IMPL to 0x3
ahci ahci.0: AHCI 0001.0100 32 slots 2 ports 3 Gbps 0x3 impl platform mode
ahci ahci.0: flags: ncq sntf pm led clo only pmp pio slum part ccc
scsi0 : ahci_platform
scsi1 : ahci_platform
ata1: SATA max UDMA/133 mmio [mem 0x4a140000-0x4a150fff] port 0x100 irq 16
ata2: SATA max UDMA/133 mmio [mem 0x4a140000-0x4a150fff] port 0x180 irq 16
m25p80 spi1.0: found m25p05-nonjedec, expected w25x32
m25p80 spi1.0: m25p05-nonjedec (64 Kbytes)
Creating 4 MTD partitions on "spi_flash":
0x000000000000-0x000000040000 : "U-Boot"
mtd: partition "U-Boot" extends beyond the end of device "spi_flash" -- size truncated to 0x10000
0x000000010000-0x000000012000 : "U-Boot Env"
mtd: partition "U-Boot Env" is out of reach -- disabled
0x000000000000-0x000000280000 : "Kernel"
mtd: partition "Kernel" extends beyond the end of device "spi_flash" -- size truncated to 0x10000
0x000000010000-0x000000010000 : "File System"
mtd: partition "File System" is out of reach -- disabled
omap2-nand driver initializing
ONFI flash detected
ONFI param page 0 valid
NAND device: Manufacturer ID: 0x2c, Chip ID: 0xca (Micron NAND 256MiB 3,3V 16-bit)
Creating 5 MTD partitions on "omap2-nand.0":
0x000000000000-0x000000260000 : "U-Boot"
0x000000260000-0x000000280000 : "U-Boot Env"
0x000000280000-0x0000006c0000 : "Kernel"
0x0000006c0000-0x00000cee0000 : "File System"
0x00000cee0000-0x000010000000 : "Reserved"
usb 1-1: new low speed USB device using musb-hdrc and address 2
davinci_mdio davinci_mdio.0: davinci mdio revision 1.6
davinci_mdio davinci_mdio.0: detected phy mask fffffff9
davinci_mdio.0: probed
davinci_mdio davinci_mdio.0: phy[1]: device 0:01, driver unknown
davinci_mdio davinci_mdio.0: phy[2]: device 0:02, driver unknown
usbcore: registered new interface driver cdc_ether
usbcore: registered new interface driver dm9601
Initializing USB Mass Storage driver...
usbcore: registered new interface driver usb-storage
USB Mass Storage support registered.
mice: PS/2 mouse device common for all mice
omap_rtc omap_rtc: rtc core: registered omap_rtc as rtc0
i2c /dev entries driver
Linux video capture interface: v2.00
usbcore: registered new interface driver uvcvideo
USB Video Class driver (v1.0.0)
OMAP Watchdog Timer Rev 0x00: initial timeout 60 sec
usbcore: registered new interface driver usbhid
usbhid: USB HID core driver
usbcore: registered new interface driver snd-usb-audio
asoc: tlv320aic3x-hifi <-> davinci-mcasp.2 mapping ok
ALSA device list:
#0: TI81XX EVM
TCP cubic registered
NET: Registered protocol family 17
VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3
omap_voltage_late_init: Voltage driver support not added
Power Management for TI81XX.
smartreflex smartreflex: Driver initialized
omap_rtc omap_rtc: setting system clock to 2000-01-01 00:00:00 UTC (946684800)
ata1: SATA link down (SStatus 0 SControl 300)
ata2: SATA link down (SStatus 0 SControl 300)
Waiting 5sec before mounting root device...
usb 1-1: New USB device found, idVendor=062a, idProduct=0003
usb 1-1: New USB device strings: Mfr=1, Product=2, SerialNumber=0
usb 1-1: Product: Optical Mouse
usb 1-1: Manufacturer: MosArt
input: MosArt Optical Mouse as /devices/platform/omap/ti81xx-usbss/musb-hdrc.0/usb1/1-1/1-1:1.0/input/input0
generic-usb 0003:062A:0003.0001: input: USB HID v1.10 Mouse [MosArt Optical Mouse] on usb-musb-hdrc.0-1/input0
mmc0: new high speed SDHC card at address 1234
mmcblk0: mmc0:1234 SA04G 3.68 GiB
mmcblk0: p1 p2
EXT3-fs: barriers not enabled
kjournald starting. Commit interval 5 seconds
EXT3-fs (mmcblk0p2): using internal journal
EXT3-fs (mmcblk0p2): recovery complete
EXT3-fs (mmcblk0p2): mounted filesystem with writeback data mode
VFS: Mounted root (ext3 filesystem) on device 179:2.
devtmpfs: mounted
Freeing init memory: 200K
INIT: version 2.86 booting
Please wait: booting...
Error opening /dev/fb0: No such file or directory
Starting udev
udevd (73): /proc/73/oom_adj is deprecated, please use /proc/73/oom_score_adj instead.
Remounting root file system...
Caching udev devnodes
NET: Registered protocol family 10
ALSA: Restoring mixer settings...
Configuring network interfaces... No state is present for card EVM
Found hardware: "" "" "" "" ""
Hardware is initialized using a generic method
No state is present for card EVM
davinci_mdio davinci_mdio.0: resetting idled controller
net eth0: attached PHY driver [Generic PHY] (mii_bus:phy_addr=0:01, id=282f014)
ADDRCONF(NETDEV_UP): eth0: link is not ready
udhcpc (v1.13.2) started
Sending discover...
PHY: 0:01 - Link is Up - 1000/Full
ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready
Sending discover...
Sending select for 192.168.20.39...
Lease of 192.168.20.39 obtained, lease time 3600
adding dns 192.168.20.238
adding dns 192.168.20.235
done.
Setting up IP spoofing protection: rp_filter.
Thu Nov 10 21:26:00 UTC 2011
INIT: Entering runlevel: 5
Loading HDVICP2 Firmware
DM816X prcm_config_app version: 2.0.0.1
Doing PRCM settings...
PRCM for IVHD0 is in Progress, Please wait.....
BW Phy Addr : 0x48180600 Data : 0x00000002
AW Phy Addr : 0x48180600 Data : 0x00000002
Phy Addr : 0x48180c04 Data : 0x00000037
BW Phy Addr : 0x48180620 Data : 0x00070000
AW Phy Addr : 0x48180620 Data : 0x00070002
BW Phy Addr : 0x48180624 Data : 0x00030000
AW Phy Addr : 0x48180624 Data : 0x00010002
Phy Addr : 0x48180600 Data : 0x00000102
BW Phy Addr : 0x48180c10 Data : 0x00000007
AW Phy Addr : 0x48180c10 Data : 0x00000003
Phy Addr : 0x48180c14 Data : 0x00000004
BW Phy Addr : 0x58088000 Data : 0x02dd0a95
AW Phy Addr : 0x58088000 Data : 0xeafffffe
BW Phy Addr : 0x58098000 Data : 0x480883c2
AW Phy Addr : 0x58098000 Data : 0xeafffffe
BW Phy Addr : 0x48180c10 Data : 0x00000003
AW Phy Addr : 0x48180c10 Data : 0x00000000
Phy Addr : 0x48180c14 Data : 0x00000007
PRCM for IVHD0 is Done Successfully
PRCM for IVHD1 is in Progress, Please wait.....
BW Phy Addr : 0x48180700 Data : 0x00000002
AW Phy Addr : 0x48180700 Data : 0x00000002
Phy Addr : 0x48180d04 Data : 0x00000037
BW Phy Addr : 0x48180720 Data : 0x00070000
AW Phy Addr : 0x48180720 Data : 0x00050002
BW Phy Addr : 0x48180724 Data : 0x00030000
AW Phy Addr : 0x48180724 Data : 0x00010002
Phy Addr : 0x48180700 Data : 0x00000102
BW Phy Addr : 0x48180d10 Data : 0x00000007
AW Phy Addr : 0x48180d10 Data : 0x00000003
Phy Addr : 0x48180d14 Data : 0x00000004
BW Phy Addr : 0x5a088000 Data : 0xafae0ea4
AW Phy Addr : 0x5a088000 Data : 0xeafffffe
BW Phy Addr : 0x5a098000 Data : 0x60aecd4c
AW Phy Addr : 0x5a098000 Data : 0xeafffffe
BW Phy Addr : 0x48180d10 Data : 0x00000003
AW Phy Addr : 0x48180d10 Data : 0x00000000
Phy Addr : 0x48180d14 Data : 0x00000007
PRCM for IVHD1 is Done Successfully
PRCM for IVHD2 is in Progress, Please wait.....
BW Phy Addr : 0x48180800 Data : 0x00000002
AW Phy Addr : 0x48180800 Data : 0x00000002
Phy Addr : 0x48180e04 Data : 0x00000037
BW Phy Addr : 0x48180820 Data : 0x00070000
AW Phy Addr : 0x48180820 Data : 0x00050002
BW Phy Addr : 0x48180824 Data : 0x00030000
AW Phy Addr : 0x48180824 Data : 0x00010002
Phy Addr : 0x48180800 Data : 0x00000102
BW Phy Addr : 0x48180e10 Data : 0x00000007
AW Phy Addr : 0x48180e10 Data : 0x00000003
Phy Addr : 0x48180e14 Data : 0x00000004
BW Phy Addr : 0x53088000 Data : 0x38ebe6ff
AW Phy Addr : 0x53088000 Data : 0xeafffffe
BW Phy Addr : 0x53098000 Data : 0xab40921f
AW Phy Addr : 0x53098000 Data : 0xeafffffe
BW Phy Addr : 0x48180e10 Data : 0x00000003
AW Phy Addr : 0x48180e10 Data : 0x00000000
Phy Addr : 0x48180e14 Data : 0x00000007
PRCM for IVHD2 is Done Successfully
PRCM Initialization completed
SysLink version : 2.00.04.83
SysLink module created on Date:Nov 10 2011 Time:19:41:10
FIRMWARE: Memory map bin file not passed
Usage : firmware_loader <Processor Id> <Location of Firmware> <start|stop> [Location of Mem map bin file]
FIRMWARE: Default memory configuration is used
MemCfg: DCMM (Dynamically Configurable Memory Map) Version : 2.1.1.1
FIRMWARE: Memory Configuration status : In Progress
FIRMWARE: 1 start Successful
Loading HDVPSS Firmware
FIRMWARE: Memory map bin file not passed
Usage : firmware_loader <Processor Id> <Location of Firmware> <start|stop> [Location of Mem map bin file]
FIRMWARE: Default memory configuration is used
MemCfg: DCMM (Dynamically Configurable Memory Map) Version : 2.1.1.1
FIRMWARE: Memory Configuration status : In Progress
FIRMWARE: 2 start Successful
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
VPSS_CORE : Failed to init fvid2 interface,
vpss: probe of vpss failed with error -22
VPSS_CORE : failed to register ti81xx-vpss driver
FATAL: Error inserting vpss (/lib/modules/2.6.37/kernel/drivers/video/ti81xx/vpss/vpss.ko): No such device
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
VPSS_CORE : Failed to init fvid2 interface,
vpss: probe of vpss failed with error -22
VPSS_CORE : failed to register ti81xx-vpss driver
FATAL: Error inserting ti81xxfb (/lib/modules/2.6.37/kernel/drivers/video/ti81xx/ti81xxfb/ti81xxfb.ko): No suc
h device
open /dev/fb0: No such file or directory
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
VPSS_CORE : Failed to init fvid2 interface,
vpss: probe of vpss failed with error -22
VPSS_CORE : failed to register ti81xx-vpss driver
FATAL: Error inserting ti81xxhdmi (/lib/modules/2.6.37/kernel/drivers/video/ti81xx/ti81xxhdmi/ti81xxhdmi.ko):
No such device
Starting system message bus: dbus.
Starting telnet daemon.
Starting syslogd/klogd: done
Starting thttpd.
open /dev/fb0: No such file or directory
open /dev/fb0: No such file or directory
expr: syntax error
Linux Frame Buffer Device Configuration Version 2.1 (23/06/1999)
(C) Copyright 1995-1999 by Geert Uytterhoeven


Usage: fbset [options] [mode]

Valid options:
General options:
-h, --help : display this usage information
--test : don't change, just test whether the mode is valid
-s, --show : display video mode settings
-i, --info : display all frame buffer information
-v, --verbose : verbose mode
-V, --version : print version information
-x, --xfree86 : XFree86 compatibility mode
-a, --all : change all virtual consoles on this device
Frame buffer special device nodes:
-fb <device> : processed frame buffer device
(default is /dev/fb0)
Video mode database:
-db <file> : video mode database file
(default is /etc/fb.modes)
Display geometry:
-xres <value> : horizontal resolution (in pixels)
-yres <value> : vertical resolution (in pixels)
-vxres <value> : virtual horizontal resolution (in pixels)
-vyres <value> : virtual vertical resolution (in pixels)
-depth <value> : display depth (in bits per pixel)
-nonstd <value> : select nonstandard video mode
-g, --geometry ... : set all geometry parameters at once
-match : set virtual vertical resolution by virtual resolution
Display timings:
-pixclock <value> : pixel clock (in picoseconds)
-left <value> : left margin (in pixels)
-right <value> : right margin (in pixels)
-upper <value> : upper margin (in pixel lines)
-lower <value> : lower margin (in pixel lines)
-hslen <value> : horizontal sync length (in pixels)
-vslen <value> : vertical sync length (in pixel lines)
-t, --timings ... : set all timing parameters at once
Display flags:
-accel <value> : hardware text acceleration enable (false or true)
-hsync <value> : horizontal sync polarity (low or high)
-vsync <value> : vertical sync polarity (low or high)
-csync <value> : composite sync polarity (low or high)
-gsync <value> : synch on green (false or true)
-extsync <value> : external syncnotify_shm_drv_sendevent failed! status = 0xfffffff0 enable (false o
notify_send_event failed! status = 0xfffffff0r true)
-bcast <value> : broadcast enable (false or true)
-laced <value> : interlace enable (false or true)
-double <value> : doublescan enable (false or true)
-rgba <r,g,b,a> : recommended length of color entries
-grayscale <value> : grayscale enable (false or true)
Display positioning:
-move <direction> : move the visible part (left, right, up or down)
-step <value> : step increment (in pixels or pixel lines)
(default is 8 horizontal, 2 vertical)
Starting PVR

notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
VPSS_CORE : Failed to init fvid2 interface,
vpss: probe of vpss failed with error -22
VPSS_CORE : failed to register ti81xx-vpss driver
FATAL: Error inserting omaplfb (/lib/modules/2.6.37/kernel/drivers/gpu/pvr/omaplfb.ko): No such device
/dev/mem opened.
Memory mapped at address 0x4036b000.
Read at address 0x48180F04 (0x4036bf04): 0x00000001
Write at address 0x48180F04 (0x4036bf04): 0x00000000, readback 0x00000000
/dev/mem opened.
Memory mapped at address 0x4025b000.
Read at address 0x48180900 (0x4025b900): 0x00000102
Write at address 0x48180900 (0x4025b900): 0x00000002, readback 0x00000002
/dev/mem opened.
Memory mapped at address 0x402b0000.
Read at address 0x48180920 (0x402b0920): 0x00040002
Write at address 0x48180920 (0x402b0920): 0x00000002, readback 0x00000002
Starting Matrix GUI application.

_____ _____ _ _
| _ |___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_
| | _| .'| . | . | | __| _| . | | | -_| _| _|
|__|__|_| |__,|_ |___| |__| |_| |___|_| |___|___|_|
|___| |___|

Arago Project http://arago-project.org dm816x-evm ttyO2

Arago 2011.09 dm816x-evm ttyO2



  • Hi Perry,

      Seeing the console output, the kernel boot commands doesn't contain the boot parameter "notifyk.vpssm3_sva=0xBF900000". Kindly add them to bootargs

    Regarding the "saveenv" command, it should work fine with switch SW4 having NAND as ON. I don't know why is it not working for you.

    Regarding the NFS problem, kindly can you post the console output.

    Regards,

    Amarinder

  • Hi Amarinder,

    Thanks a lot of your reply. I have resolved the other issues except the "saveenv" to NAND flash issue.

    Whenever I changed an environment variable in u-boot and tried to save it, I got the following warning and the console just hang forever.

    TI8168_EVM#setenv bootdelay 4
    TI8168_EVM#saveenv
    Saving Environment to NAND...
    Erasing Nand...
    Warning: Erase size 0x00002000 smaller than one erase block 0x00020000
    Erasing 0x00020000 instead

    I also noticed that the following warning messages in console output. I don't remember seeing it in previous EZSDK release.
    If it is the issue, how to get it resolved?

    NAND:  HW ECC Hamming Code selected
    NAND device: Manufacturer ID: 0x2c, Chip ID: 0xca (Micron NAND 256MiB 3,3V 16-bit)
    NAND bus width 8 instead 16 bit
    No NAND device found!!!
    0 MiB
    *** Warning - bad CRC or NAND, using default environment

    -Perry
  • Add a bit of info with remaining NAND flash issue.

    My DM816x evm board uses old silicon. The latest ezsdk supports new 2.0 silicon. Could it be that some low level code works on new silicon, but not on old ones?

     

    -Perry

  • Perry,

     

    "Warning: Erase size 0x00002000 smaller than one erase block 0x00020000

             Erasing 0x00020000 instead"
    Since the nand  eraseblock is of 0x20000 size, an erase operation can not be performed for a size value lower than that. 
    That is the reason for this warning message to come up.
    
    
    
    
    "NAND device: Manufacturer ID: 0x2c, Chip ID: 0xca (Micron NAND 256MiB 3,3V 16-bit)
    NAND bus width 8 instead 16 bit"
    Patches have been pushed in Uboot and Kernel to incorporate support for both 8 and 16 bit Nand. 
    To differentiate between the two, the CS0BW switch has to be toggled (OFF state for 16 bit nand, ON state for 8 bit nand). 
    If the switch position and Nand part don't match, such an error is shown.
    (This is also mentioned in our release notes).
    
    
    Regards,
    Parth
  • Thanks Parth. This addressed the problem.

    I assume the release notes you mentioned would be <<DM816x EZSAK 5.03 Release Notes>>. I double checked it and still didn't see anything about NAND code change mentioned there. I just want to make sure I will not miss such important information next time.

    Althrough setting bit CS0BW  to 0 resolved the NAND issue that I encountered, this unfortunately triggered another issue. The TI's ROM code already use this bit to decide PCIe BAR size. The same bit was double defined for two different purpose.  This confused me because I want both NAND and PCIE to work.

    -Perry

     

     

     

  • Perry,

    The information was mentioned in our release notes. You can also refer to the information in the 'Read this first' section of the following link:

    http://processors.wiki.ti.com/index.php/DM816x_AM389x_PSP_04.00.01.13_Release_Notes

    Regards,

    Parth

  • Thanks for the info, Parth.

    I will definitely remember to check multiple release notes and online documentation also. It seems that TI has already aware of the conflict issue with hardware switch. Hopefully it will be resolved in future release because PCIe feature is also very important to our application.

    -Perry

     

  • , if I am not mistaken, you should update SPRUGX8 – 1 July 2011 document so that it reflects DM8168-s reality. I have been doing some tests, and I think GPMC_CONFIG1_1 bits 13 and 12 (DEVICESIZE) are behaving differently in the part that I am testing than in the datasheet.

    In U-Boot code drivers/mtd/nand/ti81xx_nand.c and drivers/mtd/nand/omap_gpmc.c, original code is written this way:

    if ((readl(&gpmc_cfg->cs[cs].config1) & 0x3000) == 0x1000)

    {

    printf ("Buswidth Set to 16 bit.\n"); // ADDED BY ME

    nand->options |= NAND_BUSWIDTH_16;

    }

    In the Kernel, you can find the following code lines (in arch/arm/mach-omap2/board-ti8168evm.c): 

    		u32 *control_status = TI81XX_CTRL_REGADDR(0x40);
    if (*control_status & (1<<16))
    {
    printk (KERN_ERR "8 bit buswidth\n");
    bw = 0; /*8-bit nand if BTMODE BW pin on board is ON*/
    }
    else
    {
    printk (KERN_ERR "16 bit buswidth\n");
    bw = 2; /*16-bit nand if BTMODE BW pin on board is OFF*/
    }
    
    
    If I boot my board with CS0BW pulled up, I get nothing in U-Boot and "8 bit buswidth" message on Kernel.
    If I boot my board with CS0BW pulled down, I get "Buswidth Set to 16bit." in U-Boot and "16 bit buswidth" on Kernel boot.
    If I change U-Boot code to this:

    if ((readl(&gpmc_cfg->cs[cs].config1) & 0x3000) == 0x0000) // <== MODIFIED BY ME

    {

    printf ("Buswidth Set to 8 bit.\n"); // ADDED BY ME

    }

    I get "Buswidth Set to 8 bit." on U-Boot with CS0BW pulled up.

    This means that contrary to what the document says, GPMC_CONFIG1_1->DEVICESIZE 0h corresponds to CONTROL_STATUS->BW 1h, and vice versa. Can you confirm this?

  • OK, I have just realized of the existence of the get_sysboot_bw() function in arch/arm/cpu/arm_cortexa8/ti81xx/sys_info.c file. That is, along with the new philosophy of  CS0BW=0 -> 16 bit buswidth what causes both registers to contain opposite values. Anyhow, shouldn't the datasheet be updated in order not to lead to confusion as it has happened to me today?

  • Xabier,

    We had programmed CS0BW switch as 0 for 16bit and 1 for 8bit NAND earlier. This was done with the intention of maintaining backward compatibility, as before that, only 16bit NAND was supported (and CS0BW was set to 0 in our boot switch settings). The same was also clearly highlighted in our release notes.

    However, on coming across multiple queries regarding usage of CS0BW not in-line with the TRM, we have now programmed the CS0BW switch in accordance with the TRM document (that is, 0 for 8bit and 1 for 16bit NAND). These changes are pushed to the Arago tree and the corresponding PSP release will soon be out. The new settings are also clearly highlighted in the new release notes.

    Regards,

    Parth

  • Thank you very much for the information, Parth.

    Regards.

    Xabier.