Tool/software:
Hello all,
I tried to boot from the EMMC boot partition(mmcblk0boot0), had copied the these 3 files tiboot3, tispl.bin and u-boot.img at the specified boot partition but it exceeded the memory region.
After repowering it is trying to boot from EMMC but getting stuck as shown in the image.
Please let me know the procedure to recover the board
U-Boot SPL 2023.04-g (Feb 07 2024 - 18:06:05 +0000)
EEPROM not available at 0x56, trying to read at 0x57
Reading on-board EEPROM at 0x57 failed -1
SYSFW ABI: 3.1 (firmware rev 0x0009 '9.1.8--v09.01.08 (Kool Koala)')
Trying to boot from MMC1
MMC: block number 0x3001 exceeds max(0x2000)
mmc_load_image_raw_sector: mmc block read error
** Partition 1 not valid on device 0 **
spl_register_fat_device: fat register err - -1
spl_load_image_fat: error reading image u-boot.img, err - -1
SPL: failed to boot from all boot devices
### ERROR ### Please RESET the board ###