Tool/software:
Hi experts,
Q1: Is the maximum current consumption of CVDDRTC specified?
Q2: Also, is it within the range of the product specification that 76~120uA flows through CVDDRTC?
We are currently discussing this matter with your company's Theeban under CPR No.CPR251117003.
A customer is using C5535, but the current consumption of CVDDRTC when powered off is higher than before, which is causing a problem.
Previous standard value: 75uA or less
Abnormal value: 76~120uA
Number of units: 3.67% (424/11,541pcs)
First, I would like to confirm the product specification, so please answer Q1 and Q2..
Best regards,
O.H