Hi all,
I am new to the forums and to TI Davinci. I am having some problems booting to the NFS from my device. Maybe someone can help point me in the right direction?
I have Windows running my TFTP server (IP 192.168.0.2). This works fine. I have a VM (Ubuntu 11.04) with the NFS, I can mount the NFS and it goes well from Linux (IP 192.168.0.50). All packages (DVSDK, C6X, etc) are fresh downloads and builds. I have followed the directions in the Gettings Started Guide, but I cannot seem to boot the NFS for some reason. My EVM is 192.168.0.100 and can ping both the TFTP and the Linux VM. TFTP goes well and starts the Linux boot, but then fails when it gets to mounting the NFS. Firewall is off, NFS is running. When I look at a wireshark capture, the EVM doesn't seem to even try to go out on the network and connect to the NFS. Anyone seen this before or could help point me in the right direction I would be greatly appreciative! I have been working on this and surfing the net for help for 3 days. Below is the following output from the boot process. I have also added rootdelay=5 to the following with no help.
printenv
bootdelay=3
baudrate=115200
ethaddr=00:0e:99:02:51:54
bootfile=uImage
nfhost=192.168.1.99
videostd=ntsc
rootpath=/home/user/workdir/filesys
ipgateway=192.168.0.1
nfshost=192.168.0.50
autoload=no
filesize=1ec0b0
fileaddr=80700000
gatewayip=192.168.0.1
netmask=255.255.255.0
ipaddr=192.168.0.100
serverip=192.168.0.2
bootargs=console=ttyS0,115200n8 noinitrd rw ip=192.168.0.100:192.168.0.50:192.168.0.1:255
.255.255.0:::off eth=00:0e:99:02:51:54 root=/dev/nfs nfsroot=192.168.0.50:/home/user/work
dir/filesys,nolock rootdelay=5 mem=120M
bootcmd=tftpboot 0x80700000 uImage;bootm
stdin=serial
stdout=serial
stderr=serial
Environment size: 603/131068 bytes
Ruiva-Dm6446-0012# ping 192.168.0.2
host 192.168.0.2 is alive
Ruiva-Dm6446-0012# ping 192.168.0.50
host 192.168.0.50 is alive
Ruiva-Dm6446-0012# boot
TFTP from server 192.168.0.2; our IP address is 192.168.0.100
Filename 'uImage'.
Load address: 0x80700000
Loading: #################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#####
done
Bytes transferred = 2017372 (1ec85c hex)
## Booting image at 80700000 ...
Image Name: Linux-2.6.18_pro500-davinci_evm-
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 2017308 Bytes = 1.9 MB
Load Address: 80008000
Entry Point: 80008000
Verifying Checksum ... OK
OK
Starting kernel ...
Uncompressing Linux......................................................................
............................................................... done, booting the kernel.
Linux version 2.6.18_pro500-davinci_evm-arm_v5t_le (user@ubuntu) (gcc version 4.2.0 (Mont
aVista 4.2.0-16.0.32.0801914 2008-08-30)) #1 PREEMPT Fri Nov 25 01:32:23 EST 2011
CPU: ARM926EJ-S [41069265] revision 5 (ARMv5TEJ), cr=00053177
Machine: DaVinci EVM
Memory policy: ECC disabled, Data cache writeback
DaVinci DM6443 variant 0x1
CPU0: D VIVT write-back cache
CPU0: I cache: 16384 bytes, associativity 4, 32 byte lines, 128 sets
CPU0: D cache: 8192 bytes, associativity 4, 32 byte lines, 64 sets
Built 1 zonelists. Total pages: 30720
Kernel command line: console=ttyS0,115200n8 noinitrd rw ip=192.168.0.100:102.168.0.50:192
.168.0.1:255.255.255.0:::off eth=00:0e:99:02:51:54 root=/dev/nfs nfsroot=192.168.0.50:/ho
me/user/workdir/filesys,nolock mem=120M
TI DaVinci EMAC: Kernel Boot params Eth address: 00:0e:99:02:51:54
PID hash table entries: 512 (order: 9, 2048 bytes)
Clock event device timer0_0 configured with caps set: 03
Console: colour dummy device 80x30
Dentry cache hash table entries: 16384 (order: 4, 65536 bytes)
Inode-cache hash table entries: 8192 (order: 3, 32768 bytes)
Memory: 120MB = 120MB total
Memory: 117376KB available (3457K code, 689K data, 172K init)
Security Framework v1.0.0 initialized
Capability LSM initialized
Mount-cache hash table entries: 512
CPU: Testing write buffer coherency: ok
NET: Registered protocol family 16
DaVinci: 71 gpio irqs
WARNING: both IDE and NOR flash are enabled, but share pins.
Disable IDE for NOR support.
ch0 default output "COMPOSITE", mode "NTSC"
MUX: initialized LOEEN
MUX: initialized LFLDEN
VPBE Encoder Initialized
LogicPD encoder initialized
SCSI subsystem initialized
usbcore: registered new driver usbfs
usbcore: registered new driver hub
NET: Registered protocol family 2
IP route cache hash table entries: 1024 (order: 0, 4096 bytes)
TCP established hash table entries: 4096 (order: 2, 16384 bytes)
TCP bind hash table entries: 2048 (order: 1, 8192 bytes)
TCP: Hash tables configured (established 4096 bind 2048)
TCP reno registered
davinci_spi_board_init: NO spi support
VFS: Disk quotas dquot_6.5.1
Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
squashfs: version 3.1 (2006/08/19) Phillip Lougher
JFFS2 version 2.2. (NAND) (C) 2001-2006 Red Hat, Inc.
yaffs Nov 26 2011 23:31:37 Installing.
SGI XFS with no debug enabled
Initializing Cryptographic API
io scheduler noop registered
io scheduler anticipatory registered (default)
LTT : ltt-facilities init
LTT : ltt-facility-core init in kernel
davincifb davincifb: dm_osd0_fb: 720x480x16@0,0 with framebuffer size 675KB
davincifb davincifb: dm_vid0_fb: 0x0x16@0,0 with framebuffer size 1020KB
davincifb davincifb: dm_osd1_fb: 720x480x4@0,0 with framebuffer size 675KB
davincifb davincifb: dm_vid1_fb: 0x0x16@0,0 with framebuffer size 1020KB
davincifb davincifb.0: dm_osd0_fb: Failed to obtain ownership of OSD window.
DAVINCI-WDT: DaVinci Watchdog Timer: heartbeat 60 sec
Serial: 8250/16550 driver $Revision: 1.90 $ 2 ports, IRQ sharing disabled
serial8250.0: ttyS0 at MMIO map 0x1c20000 mem 0xfec20000 (irq = 40) is a 16550A
RAMDISK driver initialized: 1 RAM disks of 32768K size 1024 blocksize
netconsole: not configured, aborting
TI DaVinci EMAC: MAC address is 57:c0:48:7d:57:c0
TI DaVinci EMAC Linux version updated 4.0
TI DaVinci EMAC: Installed 1 instances.
Linux video capture interface: v2.00
vpfe vpfe.1: DaVinci v4l2 capture driver V1.0 loaded
Trying to register davinci display video device.
layer=c7491600,layer->video_dev=c7491760
Trying to register davinci display video device.
layer=c7491400,layer->video_dev=c7491560
davinci_init:DaVinci V4L2 Display Driver V1.0 loaded
Davici AEW Driver cannot be loaded
VIDEO PORT is not enabledData Flow path from CCDC is disabled
Davinci AF driver cannot be loaded
VIDEO PORT is not enabled
CCDC needs to be configured<6>i2c /dev entries driver
Uniform Multi-Platform E-IDE driver Revision: 7.00alpha2
ide: Assuming 50MHz system bus speed for PIO modes; override with idebus=xx
MUX: initialized HDIREN
MUX: initialized ATAEN
ide0: MMIO-DMA , BIOS settings: hda:pio, hdb:pio
Palm Chip BK3710 IDE Register Fail
Initializing USB Mass Storage driver...
usbcore: registered new driver usb-storage
USB Mass Storage support registered.
usbcore: registered new driver usbhid
drivers/usb/input/hid-core.c: v2.6:USB HID core driver
musb_hdrc: version 6.0, cppi-dma, host, debug=0
musb_hdrc musb_hdrc: No DMA interrupt line
musb_hdrc: USB Host mode controller at c805e000 using DMA, IRQ 12
musb_hdrc musb_hdrc: MUSB HDRC host driver
musb_hdrc musb_hdrc: new USB bus registered, assigned bus number 1
usb usb1: configuration #1 chosen from 1 choice
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
mice: PS/2 mouse device common for all mice
rtc_davinci_evm rtc_davinci_evm: rtc intf: proc
rtc_davinci_evm rtc_davinci_evm: rtc intf: dev (254:0)
rtc_davinci_evm rtc_davinci_evm: rtc core: registered rtc_davinci_evm as rtc0
rtc0: hours 12-23 are misreported as duplicate hours 00-11
davinci-mmc davinci-mmc.0: Supporting 4-bit mode
davinci-mmc davinci-mmc.0: Using DMA mode
Advanced Linux Sound Architecture Driver Version 1.0.12rc1 (Thu Jun 22 13:55:50 2006 UTC)
.
ASoC version 0.13.1
MUX: initialized MCBSP
AIC3X Audio Codec 0.1
asoc: aic3x <-> davinci-i2s mapping ok
ALSA device list:
#0: DaVinci EVM (aic3x)
IPv4 over IPv4 tunneling driver
TCP bic registered
NET: Registered protocol family 1
NET: Registered protocol family 17
Time: timer0_1 clocksource has been installed.
Clock event device timer0_0 configured with caps set: 08
Switched to high resolution mode on CPU 0
rtc_davinci_evm rtc_davinci_evm: hctosys: invalid date/time
usb 1-1: new high speed USB device using musb_hdrc and address 2
usb 1-1: configuration #1 chosen from 1 choice
hub 1-1:1.0: USB hub found
hub 1-1:1.0: 2 ports detected
IP-Config: Complete:
device=eth0, addr=192.168.0.100, mask=255.255.255.0, gw=192.168.0.1,
host=192.168.0.100, domain=, nis-domain=(none),
bootserver=102.168.0.50, rootserver=192.168.0.50, rootpath=
Looking up port of RPC 100003/2 on 192.168.0.50
portmap: server 192.168.0.50 not responding, timed out
Root-NFS: Unable to get nfsd port number from server, using default
Looking up port of RPC 100005/1 on 192.168.0.50
portmap: server 192.168.0.50 not responding, timed out
Root-NFS: Unable to get mountd port number from server, using default
mount: server 192.168.0.50 not responding, timed out
Root-NFS: Server returned error -5 while mounting /home/user/workdir/filesys
VFS: Unable to mount root fs via NFS, trying floppy.
VFS: Cannot open root device "nfs" or unknown-block(2,0)
Please append a correct "root=" boot option
Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(2,0)
Thanks for any help and pointing me in the right direction.
also, Maybe this is easier somehow if I can boot to a local filesystem stored in NAND? Anyone know how I might go about doing that?
Thanks
Tim