Other Parts Discussed in Thread: TLV320AIC3254
hi ,
I am working on DM37xx EVM , kernel 2.6.32 and TI Gingerbread 2.3.4 .
and use TLV320AIC3254 audio codec.
we are facing a problem in SIP call .
when we initiate a SIP call then services ( Audio flinger , media server ) has been died when ALSA try to play RINGTONE.
following are the logs that comes during SIP call.
D/AudioHardwareInterface( 988): setMode(RINGTONE)
D/TIALSAModule( 988): route called for devices 00000000 in mode 1...
E/TIALSAModule( 988): Why are we routing to a device that isn't supported by this object?!?!?!?!
D/TIALSAModule( 988): open called for devices 00000000 in mode 1...
E/TIALSAModule( 988): Unable to set buffer size to 8192: Invalid argument
I/TIALSAModule( 988): Initialized ALSA PLAYBACK device default
W/AudioPolicyManagerALSA( 988): AudioPolicyManagerALSA::getStrategyForStream() Stub Called...
W/AudioPolicyManagerALSA( 988): redirecting AudioPolicyManagerALSA::getStrategy()
D/TIALSAModule( 988): open called for devices 00000000 in mode 0...
E/TIALSAModule( 988): Failed to Initialize any ALSA PLAYBACK device: Unknown error: -16
W/AudioSystem( 1283): AudioFlinger server died!
W/IMediaDeathNotifier( 1283): media server died
W/MediaMetadataRetriever( 1259): MediaMetadataRetriever server died!
W/AudioSystem( 1282): AudioFlinger server died!
W/IMediaDeathNotifier( 1282): media server died
I/ServiceManager( 982): service 'media.audio_flinger' died
E/MediaPlayer( 1282): error (100, 0)
W/IMediaDeathNotifier( 1116): media server died
E/MediaPlayer( 1282): Error (100,0)
I/ServiceManager( 982): service 'media.player' died
I/ServiceManager( 982): service 'media.camera' died
I/ServiceManager( 982): service 'media.audio_policy' died
W/AudioSystem( 1282): AudioPolicyService server died!
W/AudioSystem( 1116): AudioFlinger server died!
W/AudioSystem( 1116): AudioPolicyService server died!
but when we received a call then after 3-4 sec , media server has been started and call is working fine .
but in this scenario we are not able to hear RINGTONE and also getting 3-5 sec delay after receiving a call.
Logs:
D/TIALSAModule( 1940): TI ALSA module opened
D/TIALSAModule( 1940): Initializing devices for TI ALSA module
I/CameraService( 1940): CameraService started (pid=1940)
D/AudioHardwareALSA( 1940): openOutputStream called for devices: 0x00000002
D/TIALSAModule( 1940): open called for devices 00000002 in mode 0...
D/StatusBarService( 1257): DISABLE_EXPAND: yes
D/StatusBarService( 1257): animateCollapse(): mExpanded=false mExpandedVisible=false mExpanded=false mAnimating=false mAnimY=0.0 mAnimVel=0.0
I/ServiceManager( 1282): Waiting for service media.audio_policy...
E/ALSAControl( 1940): Control 'HeadsetR Mixer AudioR1' cannot get element info: -2
E/ALSAControl( 1940): Control 'HeadsetL Mixer AudioL1' cannot get element info: -2
E/ALSAControl( 1940): Control 'Headset Playback Volume' cannot get element info: -2
I/TIALSAModule( 1940): Initialized ALSA PLAYBACK device default
I/AudioFlinger( 1940): AudioFlinger's thread 0x496c8 ready to run
D/TIALSAModule( 1940): route called for devices 00000002 in mode 0...
E/AudioHardwareALSA( 1940): CALLING STANDBY
E/AudioService( 1116): Media server started.
E/AudioHardwareALSA( 1940): setParameters INVALID OPERATION
D/AudioHardwareInterface( 1940): setMode(RINGTONE)
D/TIALSAModule( 1940): route called for devices 00000000 in mode 1...
E/TIALSAModule( 1940): Why are we routing to a device that isn't supported by this object?!?!?!?!
D/TIALSAModule( 1940): open called for devices 00000000 in mode 1...
E/TIALSAModule( 1940): Unable to set buffer size to 8192: Invalid argument
I/TIALSAModule( 1940): Initialized ALSA PLAYBACK device default
E/AudioHardwareALSA( 1940): setParameters INVALID OPERATION
W/AudioPolicyManagerALSA( 1940): AudioPolicyManagerALSA::getStrategyForStream() Stub Called...
W/AudioPolicyManagerALSA( 1940): redirecting AudioPolicyManagerALSA::getStrategy()
kindly suggest any solution as soon as possible because .VOIP call is critical for us