Hi,
I'm experimenting a bit with the new ti81xx xserver driver, that supports dual display. I already tried HDMI as main display + SVIDEO as secondary/extended display- That works quite well.
The question now is: How to get the ti814x-EVM's onboard LCD to work in extended desktop mode in combination with a HDMI display?
I already tried, with the following entry in the xorg.conf, but it didn't seem to work:
Section "Device"
Identifier "TI8148"
Driver "ti81xx"
EndSection
Section "Monitor"
Identifier "HDMI"
ModeLine "1920x1080" 148.500 1920 2008 2042 2200 1080 1084 1089 1125 +hsync +vsync
Option "PreferredMode" "1920x1080"
Option "Enable" "true"
EndSection
Section "Monitor"
Identifier "LCD"
ModeLine "800x480" 33.500 800 864 889 810 480 490 503 490 -hsync -vsync
Option "RightOf" "HDMI"
Option "PreferredMode" "800x480"
Option "Enable" "true"
EndSection
If you have any tip, I'd be happy to give it a new try. I'm not really sure about the modeline for the LCD.
BTW, I even tried to use the LCD as main display. The result was, let's say, not really satisfying. I can't get the LCD to display the whole desktop on my test system. It's always a bit blurry with strange colors and only showing part of the desktop.
Thank you very much in advance for any hints!
Sebastian