Other Parts Discussed in Thread: DM3730
Hi,
We're using a DM3730 on a Variscite SOM, and attempting to reflash the EBoot sector to correct some display issues using the Flash Tool v1.06/1.05. When attempting to erase the EBOOT region, on a Windows 7 machine (running app as admin), the program gives a crash error code of -1073741819 about 3 seconds after reading the asic ID. On two Windows XP machines, the application crashes alltogether after the same time period. We've attempted to use a true UART from an older XP machine, as well as FTDI USB serial adapters. Using the params AM37XX (Hynix), HWECC, ONFI Compliant, 1 bit ECC, Erase Region Offset 0x80000, size: 0x40000.
What are the hardware requirements in order for this to succeed? The Flash Wiki indicates different switches for different carrier boards, however, would like to know more details on the exact hardware signals and states required, as we don't have schematics for the carrier boards listed, ie: Mistral. Also, what are the EBoot requirements in order for this to succeed?
Please advise if additional info is needed. Thanks,
Nick