This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SK-AM62A-LP: Need expected command and throughput numbers for TCP and UDP

Part Number: SK-AM62A-LP
Other Parts Discussed in Thread: CC3351, CC3551

Tool/software:

Hi Team,
I am planning to run UDP and TCP traffics after CC3351 WLAN associated with an AP. Please review my queries and let me know.

  1. Could you please let me know -b (bandwidth) for UDP and -w (window size) for TCP?
  2. Why application speed shows only 50Mbps? the link is giving Tx 73 and Rx is 86 Mbps
  3. Is there any expected throughput numbers of TCP and UDP for Tx and Rx?

Using tool: IPERF3
SDK Ver:
root@am62axx-evm:/usr/share/cc33xx#uname -a
Linux am62axx-evm 6.6.58-ti-01497-ga7758da17c28-dirty #1 SMP PREEMPT Wed Nov 27 13:23:15 UTC 2024 aarch64 GNU/Linux
root@am62axx-evm:/usr/share/cc33xx# iw dev wlan0 link
Connected to 08:bf:b8:8f:64:a8 (on wlan0)
SSID: ASUS_GTAXE16000_2G
freq: 2437.0
RX: 867296160 bytes (4879924 packets)
TX: 2034052918 bytes (1358407 packets)
signal: -33 dBm
rx bitrate: 86.0 MBit/s HE-MCS 7 HE-NSS 1 HE-GI 0 HE-DCM 0
tx bitrate: 73.1 MBit/s HE-MCS 7 HE-NSS 1 HE-GI 2 HE-DCM 0
bss flags: short-slot-time
dtim period: 1
beacon int: 100