Hello,
I am using an AM1806 with DDR2 memory.
I think I remember reading in one of the design guides that it was not generally recommended to use the same 1.8V supply for DDR_DVDD and DVDD3318_A/B/C due to switching noise propagating from the IO banks to the DDR2 Signals. Is this in fact TI's recommendation?
Also, I have seen different implementations of the DQGATE termination resistor. For my schematic, I have 22 Ohm resistors on the D0-D15,DQS0-DQS1, and DQM0-DQM1. I have 10 Ohms on the CLKN/P lines, and no terminators on any other pin. In this case, should I add a terminator to the DQGATE trace?
Finally, is it OK to terminate the data pins and not the address pins for DDR2?
Thanks,
Charles