Part Number: CCSTUDIO
Other Parts Discussed in Thread: CC3235SF, UNIFLASH
Tool/software:
Hi,
I am working with a custom PCB using the CC3235SF and I’ve already successfully flashed my firmware using CCS (not UniFlash). After flashing:
-
I disconnected SOP1 and also unplugged the USB.
-
Then I reset the board and powered it externally.
-
I waited for 30 minutes, but I still don’t see any output on HiveMQ.
The code should publish this message when it starts:
MQTTpublish("Ready to receive... (STA/AP)");
Then I'm supposed to send either "AP" or "STA", and after that, I should receive MQTT messages with GNSS info, battery level, time, etc.
Everything works fine when I run it via CCS Debug mode — I can see the MQTT messages appearing as expected. But after flashing and running standalone, I get nothing on HiveMQ .Is there anything else I need to configure to make the CC3235SF run the code standalone from flash?