Other Parts Discussed in Thread: AM68A, AM69A, AM67A
Tool/software:
We have a medical device that works on an iPhone/iPad, where we look at the user's eyes for medical information. I would like to build a similar standalone function, where we build a small device (would like it to fit on a finger) that captures the users face, and then we store at 60Hz - 120Hz the eye structure, and process the frames in real time. Our current processing method is an AI model, so the processor would need to be able to have some sort of attached chiplet that would allow for floating point matrix functions with at least 16-24G of memory. The video would not need to be stored, except for tens of frames, possibly a hundred if feasible. Is there a small form factor camera/ai processor combination offered by TI? It could probably be 8 bit if needed.