Hi all,
Currently i am working on Appro DM368-IPNC reference design.Please help me clarify the following doubts:
1.On customised dm368 evm board steps needed to port ipnc application e.g among the submodules (av_server,system_server,osa,codec_engine,etc)which i can port easily.
with minimum interdependancy.
2.If we have to implement uboot,bootloader on our own customised evm board.How can we write it for DM368-IPNC.Any TI document which explains how to write bootloder for DM368-IPNC will be of great help.
3.Also how can we test osa,cmem,codec engine library,video capture and port ipnc application on that.
4.If the dvsdk and lsp we are using with Appro reference design we can port on our own built dm368 evm board without major modiifcations.
5.In the av_server design guide it is mentioned the steps to replace the sensor.Currently i am having DM368-IPNC IMX036 Appro design.If i open the box and replace the IMX036 with mt9m111 image sensor daughter card on the board and do the steps for replacing sensor as desribed in av_server design guide,will that work or there are changes necessary elsewhere.Moreover is that adventure feasible also.
also following issues in linux:
Please answer wrt to DM368-IPNC.
1.In which files/directory we initialize bootlog.which files i have
to
change in order to modify boot log.
how to make a process run as
daemon process.
2.Also about linux boot sequence,help/tutorial on linux boot
sequence.
3.Major steps in bringing up the new custom evm board.
4.Things
to know in order to write the bootloader.
Thanks and Regards,
Mayank