This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP-AM263: Not able to scan the EtherCAT subdevice on TwinCAT

Part Number: LP-AM263

Tool/software:

Hi Experts,

My customer is testing the beckhoff EtherCAT example, but they can not scan the subdevice.

We've checked the following output:

1. The application was build successfully

2. There is SBL output and the example output (But it's missing the CPU frequency output, is this a problem?)

3. TwinCAT driver is installed. The adapter is shown in the "installed a ready to use (for demo only)" tab.

4. The Wire is connected to the PC and the LP, we tried both port. (BTW which is port0)

5. sdk version is 10.00

6. When scan with twincat, there is no error but a no new IO device was found message