This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4AL-Q1: Crash when define large array in post process

Part Number: TDA4AL-Q1

Tool/software:

Hi, I encountered an issue when I declared the following arrays in the post-processing stage (DSP2) and tried to store the model's output into them — the program crashes, and the system even requires a full reboot before it can run programs that were previously working fine.

Could this be due to insufficient memory?

#define MAX_LANE_NUM 4

#define REG_MAT_IDX1 48
#define REG_MAT_IDX2 80
float regMat[MAX_LANE_NUM][REG_MAT_IDX1][REG_MAT_IDX2];

#define MASK_MAT_IDX1 48
#define MASK_MAT_IDX2 80
float maskMat[MAX_LANE_NUM][MASK_MAT_IDX1][MASK_MAT_IDX2];

Best regards,

Jiemin