Hello,
I have a problem with error "Your BIOS Version is not compatible with this RTA Version. It must be version 5.2.x.x. Your version looks to be : a non BIOS program , or possibly BIOS 490 or earlier"
I downloaded a a few new BIOS versions 5.2.x.x. , I updated the ccs3.3. with Service Release 12.1 (3.3.82.13),
But still getting this error. I managed to change the bios version in manager but still the same error.
I'm using matlab r2011b and CCS3.3, before that i was using CCS3.1. But because of compatibility of matlab and CCS I was forced to install 3.3.
My job is to try the reverberatipon demo in matlab and than incrment build it to CCS3.3 (it's automaticly done) . So, i will run the mp3 music from my computer directly to the input of 5510 board, and than on the output side should be the reverberation of this mp3 song. that's it! But, as you can see, i have a problem.
Please can anybody help.
What exactly is this RTA version? I'm not familiar with this.
And ofcourse if somebody had the same problem please help me! I'm allredy instaling this for two months to put this all programs to be compatibile. Yes, I'm new in this :)