Other Parts Discussed in Thread: TVP5146
This is regarding one of our new requirement of interfacing 8 bit BT.656 video with TI DSP – DM6435. Now DM6435 supports BT.656 capture for both 8-bit and 10bit mode, thus I am bit confused here regarding connection of 8-bit BT.656 from video source to DM6435 VPIF.
I am not sure which one is correct from following two statement. Can soembody please help me here ?
1. D0 [LSB] of Bt.656 source should be connected to D0 [pin name of YI0[ Pin name YI0(CCD0)/GP[36] in DM6435 ] & D8 [MSB] of Bt.656 video source should be connected to D7[ pin name of YI7(CCD7)/GP[43] in DM6435 ]
2. D0 [LSB] of Bt.656 source should be connected to D2 [pin name YI2(CCD2)/GP[38] in DM6435 ] & D8 [MSB] of Bt.656 video source should be connected to D9 [pin name of CI1(CCD9)/EM_A[19]/GP[45] in DM6435 ]