This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Appro DM368 av_server

 

Hi,

 

On running ./av_server.out D1 it is giving the option to select choices.On selecting r or y option after enabling file save option

it should lead to raw image save or yuv image save.On seeing the code i could find out that the file name is something like DATA.yuvTI

for yuv file but i am not seeing this file created anywhere in the directory.Do  have to enable some option in order to get this file created.

If it is already created at which location can i find it.Please guide.I am working on Appro DM368-IPNC.

 

Regards,

Mayank