This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

STANAG support for the H.264 encoder.

I'm trying to determine if the 8168 can handle encoding a military standard STANAG 3350, which is 640x875 resolution and would come in via the 16-bit digital bus. It looks like the encoder can be configured to support the resolution but I'd like to double check the configuration.