Hi all,
I have a problem doing more than one receive transaction using the uPP peripheral and its DMA component.
The size of one transfer is 2048 bytes. The buffer where the DMA component puts the received data to is a UInt16 buffer consisting of 1024 elements. The DMA configuration is LINECNT=1, BYTECOUNT=2048, LINEHOFFST = 0 and window address pointing to the first element of the receive buffer. Iam using just one DMA channel (channel I) and only UPP interface channel A in receive mode.
Now the first package seems to be received, I get the EOWI interrupt and can see the received data via the debugger watch window in the receive buffer. The DMA descriptors are programmed again and also the next EOWI is received. But then I can't see any change within the receive buffer (there should be one). Interestingly is that this only applies if data is read from the buffer (lets say into a local variable). If I remove this part of the code, where the data is read out, Iam able to see at least a change in the data. What can went wrong here? Do you have any ideas?
Any help on this issue would be very appreciated. I've attached the relevant code part of UPP initialization, ISR and task where the data is read out, and the DMA is reprogrammed. If you need additional information please let me
Thanks.
Kind Regards,
Steve
#include <ti/sysbios/BIOS.h>
#include <ti/sysbios/knl/Task.h>
#include <stdio.h>
#include <string.h>
#include <ti/sdo/io/DriverTypes.h>
#include <ti/sdo/edma3/drv/edma3_drv.h>
#include <ti/psp/spi/Spi.h>
#include <ti/sdo/io/Stream.h>
#include <ti/psp/cslr/cslr.h>
#include <ti/psp/cslr/cslr_upp.h>
#include <ti/psp/cslr/cslr_syscfg0_OMAPL138.h>
#include <ti/psp/cslr/soc_OMAPL138.h>
#include <ti/sysbios/family/c64p/EventCombiner.h>
#include <ti/sysbios/family/c64p/Hwi.h>
#include <ti/sysbios/ipc/Semaphore.h>
#include "common.h"
#include "fpga_util.h"
#include "fpga.h"
#include "edma.h"
#define UPP_TELEGRAM_SIZE 16
#define UPP_TELEGRAMS_IN_PACKAGE 128
#define UPP_RX_BUFFER_SIZE ((UPP_TELEGRAM_SIZE / 2) * UPP_TELEGRAMS_IN_PACKAGE)
//#define FPGA_BOOT_VIA_JTAG
static Semaphore_Handle rx_event_upp;
#pragma DATA_ALIGN(upp_rx_buffer, 8);
#pragma DATA_SECTION(upp_rx_buffer, ".upp_rx_image");
static UInt16 upp_rx_buffer[UPP_RX_BUFFER_SIZE];
static CSL_SyscfgRegsOvly syscfg0_regs = (CSL_SyscfgRegsOvly) CSL_SYSCFG_0_REGS;
static CSL_UppRegsOvly upp0_regs = (CSL_UppRegsOvly) CSL_UPP_0_REGS;
static Void UppIsr(UArg arg0);
static Void InitUpp(Void);
static Void UppIsr(UArg arg0)
{
Gpio_PinCmdArg pinCmdArg;
while (upp0_regs->UPIER != 0)
{
if (CSL_FEXT(upp0_regs->UPIER, UPP_UPIER_EOWI))
{
// Handle EOWI...
pinCmdArg.pin = GPIO_PIN_TO_DRIVER_NUMBER(6, 8);
pinCmdArg.value = 1;
Gpio_setPinVal(gpio0, &pinCmdArg, NULL);
upp0_regs->UPIER = CSL_FINS(upp0_regs->UPIER, UPP_UPIER_EOWI, TRUE);
Semaphore_post(rx_event_upp);
}
if (CSL_FEXT(upp0_regs->UPIER, UPP_UPIER_EOLI))
{
// Handle EOLI...
upp0_regs->UPIER = CSL_FINS(upp0_regs->UPIER, UPP_UPIER_EOLI, TRUE);
}
if (CSL_FEXT(upp0_regs->UPIER, UPP_UPIER_ERRI))
{
// Handle ERRI...
upp0_regs->UPIER = CSL_FINS(upp0_regs->UPIER, UPP_UPIER_ERRI, TRUE);
}
if (CSL_FEXT(upp0_regs->UPIER, UPP_UPIER_UORI))
{
// Handle UORI...
upp0_regs->UPIER = CSL_FINS(upp0_regs->UPIER, UPP_UPIER_UORI, TRUE);
}
if (CSL_FEXT(upp0_regs->UPIER, UPP_UPIER_DPEI))
{
// Handle DPEI...
upp0_regs->UPIER = CSL_FINS(upp0_regs->UPIER, UPP_UPIER_DPEI, TRUE);
}
if (CSL_FEXT(upp0_regs->UPIER, UPP_UPIER_EOWQ))
{
// Handle EOWQ...
upp0_regs->UPIER = CSL_FINS(upp0_regs->UPIER, UPP_UPIER_EOWQ, TRUE);
}
if (CSL_FEXT(upp0_regs->UPIER, UPP_UPIER_EOLQ))
{
// Handle EOLQ...
upp0_regs->UPIER = CSL_FINS(upp0_regs->UPIER, UPP_UPIER_EOLQ, TRUE);
}
if (CSL_FEXT(upp0_regs->UPIER, UPP_UPIER_ERRQ))
{
// Handle ERRQ...
upp0_regs->UPIER = CSL_FINS(upp0_regs->UPIER, UPP_UPIER_ERRQ, TRUE);
}
if (CSL_FEXT(upp0_regs->UPIER, UPP_UPIER_UORQ))
{
// Handle UORQ...
upp0_regs->UPIER = CSL_FINS(upp0_regs->UPIER, UPP_UPIER_UORQ, TRUE);
}
if (CSL_FEXT(upp0_regs->UPIER, UPP_UPIER_DPEQ))
{
// Handle DPEQ...
upp0_regs->UPIER = CSL_FINS(upp0_regs->UPIER, UPP_UPIER_DPEQ, TRUE);
}
}
upp0_regs->UPEOI = CSL_FMKT(UPP_UPEOI_EOI, DONE);
}
static Void InitUpp(Void)
{
Int i;
EventCombiner_dispatchPlug(94, &UppIsr, 0, 1);
EventCombiner_enableEvent(94);
Hwi_enableInterrupt(11);
Psc_ModuleClkCtrl(psc1, 19, Psc_moduleClkCtrl_ENABLE, NULL);
memset(upp_rx_buffer, 0, sizeof(upp_rx_buffer));
syscfg0_regs->PINMUX14 = CSL_FINST(syscfg0_regs->PINMUX14, SYSCFG_PINMUX14_PINMUX14_31_28, UPP_D10);
syscfg0_regs->PINMUX14 = CSL_FINST(syscfg0_regs->PINMUX14, SYSCFG_PINMUX14_PINMUX14_27_24, UPP_D11);
syscfg0_regs->PINMUX14 = CSL_FINST(syscfg0_regs->PINMUX14, SYSCFG_PINMUX14_PINMUX14_23_20, UPP_D12);
syscfg0_regs->PINMUX14 = CSL_FINST(syscfg0_regs->PINMUX14, SYSCFG_PINMUX14_PINMUX14_19_16, UPP_D13);
syscfg0_regs->PINMUX14 = CSL_FINST(syscfg0_regs->PINMUX14, SYSCFG_PINMUX14_PINMUX14_15_12, UPP_D14);
syscfg0_regs->PINMUX14 = CSL_FINST(syscfg0_regs->PINMUX14, SYSCFG_PINMUX14_PINMUX14_11_8, UPP_D15);
syscfg0_regs->PINMUX15 = CSL_FINST(syscfg0_regs->PINMUX15, SYSCFG_PINMUX15_PINMUX15_31_28, UPP_D2);
syscfg0_regs->PINMUX15 = CSL_FINST(syscfg0_regs->PINMUX15, SYSCFG_PINMUX15_PINMUX15_27_24, UPP_D3);
syscfg0_regs->PINMUX15 = CSL_FINST(syscfg0_regs->PINMUX15, SYSCFG_PINMUX15_PINMUX15_23_20, UPP_D4);
syscfg0_regs->PINMUX15 = CSL_FINST(syscfg0_regs->PINMUX15, SYSCFG_PINMUX15_PINMUX15_19_16, UPP_D5);
syscfg0_regs->PINMUX15 = CSL_FINST(syscfg0_regs->PINMUX15, SYSCFG_PINMUX15_PINMUX15_15_12, UPP_D6);
syscfg0_regs->PINMUX15 = CSL_FINST(syscfg0_regs->PINMUX15, SYSCFG_PINMUX15_PINMUX15_11_8, UPP_D7);
syscfg0_regs->PINMUX15 = CSL_FINST(syscfg0_regs->PINMUX15, SYSCFG_PINMUX15_PINMUX15_7_4, UPP_D8);
syscfg0_regs->PINMUX15 = CSL_FINST(syscfg0_regs->PINMUX15, SYSCFG_PINMUX15_PINMUX15_3_0, UPP_D9);
syscfg0_regs->PINMUX16 = CSL_FINST(syscfg0_regs->PINMUX16, SYSCFG_PINMUX16_PINMUX16_7_4, UPP_D0);
syscfg0_regs->PINMUX16 = CSL_FINST(syscfg0_regs->PINMUX16, SYSCFG_PINMUX16_PINMUX16_3_0, UPP_D1);
syscfg0_regs->PINMUX13 = CSL_FINST(syscfg0_regs->PINMUX13, SYSCFG_PINMUX13_PINMUX13_31_28, GPIO6_8);
syscfg0_regs->PINMUX13 = CSL_FINST(syscfg0_regs->PINMUX13, SYSCFG_PINMUX13_PINMUX13_27_24, CH1_ENABLE);
syscfg0_regs->PINMUX13 = CSL_FINST(syscfg0_regs->PINMUX13, SYSCFG_PINMUX13_PINMUX13_23_20, CH1_START);
syscfg0_regs->PINMUX13 = CSL_FINST(syscfg0_regs->PINMUX13, SYSCFG_PINMUX13_PINMUX13_19_16, CH1_CLK);
syscfg0_regs->PINMUX3 = CSL_FINST(syscfg0_regs->PINMUX3, SYSCFG_PINMUX3_PINMUX3_15_12, SPI0_SIMO0) |
CSL_FINST(syscfg0_regs->PINMUX3, SYSCFG_PINMUX3_PINMUX3_11_8, SPI0_SOMI0) |
CSL_FINST(syscfg0_regs->PINMUX3, SYSCFG_PINMUX3_PINMUX3_3_0, SPI0_CLK) |
CSL_FINST(syscfg0_regs->PINMUX3, SYSCFG_PINMUX3_PINMUX3_23_20, GPIO8_3);
upp0_regs->UPPCR = CSL_FINS(upp0_regs->UPPCR, UPP_UPPCR_SWRST, 1);
/* wait some cycles according to the doc */
for (i = 0; i < 20; i++);
upp0_regs->UPPCR = CSL_FINS(upp0_regs->UPPCR, UPP_UPPCR_SWRST, 0);
upp0_regs->UPCTL = CSL_FMKT(UPP_UPCTL_DPWA, FULL) |
CSL_FMKT(UPP_UPCTL_IWA, 16BIT) |
CSL_FMKT(UPP_UPCTL_DRA, SINGLE) |
CSL_FMKT(UPP_UPCTL_SDRTXIL, DISABLE) |
CSL_FMKT(UPP_UPCTL_CHN, ONE) |
CSL_FMKT(UPP_UPCTL_MODE, RECEIVE);
upp0_regs->UPICR = CSL_FMKT(UPP_UPICR_ENAA, ENABLE) |
CSL_FMKT(UPP_UPICR_STARTA, ENABLE) |
CSL_FMKT(UPP_UPICR_WAITPOLA, NORMAL) |
CSL_FMKT(UPP_UPICR_ENAPOLA, NORMAL) |
CSL_FMKT(UPP_UPICR_STARTPOLA, NORMAL);
upp0_regs->UPDLB = CSL_FMKT(UPP_UPDLB_BA, DISABLE) |
CSL_FMKT(UPP_UPDLB_AB, DISABLE);
upp0_regs->UPTCR = CSL_FMKT(UPP_UPTCR_RDSIZEI, 64B);
/* setup UPP and DMA interrupts */
upp0_regs->UPIES = CSL_FMKT(UPP_UPIES_EOLQ, DISABLED) |
CSL_FMKT(UPP_UPIES_EOWQ, DISABLED) |
CSL_FMKT(UPP_UPIES_ERRQ, DISABLED) |
CSL_FMKT(UPP_UPIES_UORQ, DISABLED) |
CSL_FMKT(UPP_UPIES_DPEQ, DISABLED) |
CSL_FMKT(UPP_UPIES_EOLI, DISABLED) |
CSL_FMKT(UPP_UPIES_EOWI, SET) |
CSL_FMKT(UPP_UPIES_ERRI, SET) |
CSL_FMKT(UPP_UPIES_UORI, SET) |
CSL_FMKT(UPP_UPIES_DPEI, SET);
upp0_regs->UPIER = CSL_FINS(upp0_regs->UPIER, UPP_UPIER_EOWI, TRUE);
upp0_regs->UPEOI = CSL_FMKT(UPP_UPEOI_EOI, DONE);
/* enable UPP peripheral */
upp0_regs->UPPCR = CSL_FMKT(UPP_UPPCR_EN, ENABLE) |
CSL_FMKT(UPP_UPPCR_SOFT, ENABLE) |
CSL_FMKT(UPP_UPPCR_FREE, DISABLE) |
CSL_FMKT(UPP_UPPCR_RTEMU, ENABLE);
/* setup DMA descriptors */
upp0_regs->UPID0 = CSL_FMK(UPP_UPID0_ADDRH,
(((UInt32) &upp_rx_buffer[0]) >> 3));
upp0_regs->UPID1 = CSL_FMK(UPP_UPID1_LNCNT, 1) |
CSL_FMK(UPP_UPID1_BCNTH, (UPP_RX_BUFFER_SIZE << 1) >> 1);
upp0_regs->UPID2 = CSL_FMK(UPP_UPID2_LNOFFSETH, 0);
}
Void FPGA_TaskUppDataHandler(UArg a, UArg b)
{
while (1)
{
UInt16 i;
Gpio_PinCmdArg pinCmdArg;
Semaphore_pend(rx_event_upp, BIOS_WAIT_FOREVER);
while (CSL_FEXT(upp0_regs->UPIS2, UPP_UPIS2_PEND) == CSL_UPP_UPIS2_PEND_TRUE)
{
asm(" nop");
}
i = upp_rx_buffer[0]; /* !!! durch diese Zeile funktioniert der 2. Transfer nicht mehr bzw ich kann keine Aenderungen mit dem Debugger im Speicher mehr sehen */
//memset(upp_rx_buffer, 0x00, sizeof(upp_rx_buffer));
/* setup DMA descriptors */
current_rx_buffer = (current_rx_buffer + 1) % 10;
upp0_regs->UPID0 = CSL_FMK(UPP_UPID0_ADDRH,
(((UInt32) &upp_rx_buffer[0]) >> 3));
upp0_regs->UPID1 = CSL_FMK(UPP_UPID1_LNCNT, 1) |
CSL_FMK(UPP_UPID1_BCNTH, (UPP_RX_BUFFER_SIZE << 1) >> 1);
upp0_regs->UPID2 = CSL_FMK(UPP_UPID2_LNOFFSETH, 0);
pinCmdArg.pin = GPIO_PIN_TO_DRIVER_NUMBER(6, 8);
pinCmdArg.value = 0;
Gpio_setPinVal(gpio0, &pinCmdArg, NULL);
}
}