This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Dm8148 ISS support for android

Hello,

Currently we are working with Android unofficial releases(rowboat-gingerbread-ti81xx-mc-dsp-snapshot-GMT20110926200120.xml manifest ) for the DM8148 EVM from Mistral. We are considering using camera parallel interface(ISS interface) on the DM8148 EVM and we dont see any support for ISS in both these packages. When is the planned date for pushing the support to the mainline ?

Also noticed that is no details on this interface in the TRM . Do you have any TRM information on the ISS? Is there any sample code for ISS interface which we can get as patches for our internal development?

Are the sources packages available for the HDVPSS(M3Vpss and M3Vicp2)(currently binary packages) for DM8148 ?

Looks like the current is Syslink releases (
2_00_03_82  ) the build breaks with android framework. Any updates on the version which works on DM8148 with Android releases?

What's the official date planned for Android release which supports DM8148 EVM?

 

Thanks

Mike