This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM620-Q1: Allowance of H time length for McASP's TDM input

Part Number: AM620-Q1
Other Parts Discussed in Thread: AM620

Tool/software:

I have a question about the TDM input settings for McASP.
Is it a problem that the frame sync H time is longer than 1 word when Sync Polarity is set to “Rising Edge”?
The frame sync setting of the TDM source to be connected is “H/L 50% ratio” so the H time is longer than 1 word, but I would like to confirm if this is a problem since the AM620 setting allows only 1 bit and 1 word to be selected.

Thanks Naomichi