Tool/software:
Champs:
please see the customer log, may we know how to let user know the Nand flash size even they used the SD card boot?
Thanks.
BR Rio
U-Boot SPL 2024.04-dirty (Apr 17 2025 - 17:08:26 +0800) SYSFW ABI: 4.0 (firmware rev 0x000a '10.1.8--v10.01.08 (Fiery Fox)') SPL initial stack usage: 13456 bytes CTRL_MMR0 (BootMode): 0x243 Trying to boot from MMC2 Authentication passed Authentication passed Authentication passed Authentication passed Authentication passed Starting ATF on ARM64 core... NOTICE: BL31: v2.11.0(release):v2.11.0-906-g58b25570c9-dirty NOTICE: BL31: Built : 04:20:32, Nov 1 2024 U-Boot SPL 2024.04-dirty (Apr 17 2025 - 17:08:43 +0800) SYSFW ABI: 4.0 (firmware rev 0x000a '10.1.8--v10.01.08 (Fiery Fox)') SPL initial stack usage: 1904 bytes CTRL_MMR0 (BootMode): 0x243 Trying to boot from MMC2 Authentication passed Authentication passed U-Boot 2024.04-dirty (Apr 17 2025 - 17:08:43 +0800) SoC: AM62X SR1.0 HS-FS Model: Texas Instruments AM62x LP SK EEPROM not available at 0x50, trying to read at 0x51 Board: AM62-LP-SKEVM rev E2 DRAM: 2 GiB Core: 83 devices, 32 uclasses, devicetree: separate NAND: Tony add board_nand_init tony add gpmc_nand_init tony add gpmc_nand_init in tony add gpmc_nand_init exit 0 MiB MMC: mmc@fa10000: 0, mmc@fa00000: 1 Loading Environment from NAND... tony add gpmc_nand_init tony add gpmc_nand_init in tony add gpmc_nand_init error exit nand: error: Unable to find NAND settings in GPMC Configuration - quitting tony add gpmc_nand_init tony add gpmc_nand_init in tony add gpmc_nand_init error exit nand: error: Unable to find NAND settings in GPMC Configuration - quitting *** Warning - bad CRC, using default environment In: serial Out: serial Err: serial Net: eth0: ethernet@8000000port@1 Hit any key to stop autoboot: 0 => mtdparts device spi-nand0 <spi-nand0>, # parts = 13 #: name size offset mask_flags 0: tiboot3 0x00080000 0x00000000 0 1: tispl 0x00200000 0x00080000 0 2: UBOOT 0x00400000 0x00280000 0 3: ENV 0x00100000 0x00680000 0 4: RAWDATA 0x00080000 0x00780000 0 5: DTB0 0x00080000 0x00800000 0 6: DTB1 0x00080000 0x00880000 0 7: KERNEL0 0x00a00000 0x00900000 0 8: KERNEL1 0x00a00000 0x01300000 0 9: ROOTFS0 0x00a00000 0x01d00000 0 10: ROOTFS1 0x00a00000 0x02700000 0 11: BOOT_BAK 0x00400000 0x03100000 0 12: HMI 0x04b00000 0x03500000 0 active partition: spi-nand0,0 - (tiboot3) 0x00080000 @ 0x00000000 defaults: mtdids : spi-nand0=spi-nand0 mtdparts: mtdparts=spi-nand0:512k(tiboot3),2m(tispl),4m(UBOOT),512k(ENV0),512k(ENV1),512k(RAWDATA),512k(DTB0),512k(DTB1),10m(KERNEL0),10m(KERNEL1),10m(ROOTFS0),10m(ROOTFS1),4m(BOOT_BAK),-(HMI) => sf probe => nand device 0 => nand info =>