This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3358: SPI (serial peripheral interface)

Part Number: AM3358


Tool/software:

SPI (serial peraphral interface) has two bits W1 and W0, which define number of bytes in each transfer (see below).

R/W W1 W0 A12 A11 A10 A9 A8 A7 A6 A5 A4 A3 A2 A1 A0. 

For example, W1 W0 = "00" or "01" means one byte or two bytes transfer. 

Does AM335x McSPI support this? Thank you.