Other Parts Discussed in Thread: OMAP3530
Hello,
I am trying to run the C6Accel demo application on the OMAP3530EVM from Mistral and I have a problem.
I have modified the demo applications to include the tests only for the math and fixed-point processing kernels and not any image/video kernels.
I have also modified the loadmodules_omap3530_c6accel.sh for my board's memory map. Here is the output during the loadmodules_omap3530_c6accel.sh:
CMEMK module: built on Sep 22 2009 at 10:44:38
Reference Linux version 2.6.29
File /db/rtree/install/trees/products/davincisw-h44x/imports/dvsdk_COMMON/dvsdk_3_00_02_44/linuxutils_2_24_02/packages/ti/sdo/linuxutils/cmem/src/module/cm
emk.c
ioremap_nocache(0x88300000, 16777216)=0xcb000000
allocated heap buffer 0xcb000000 of size 0xfec000
cmem initialized 1 pools between 0x88300000 and 0x89300000
DSPLINK Module (1.61.03) created on Date: Nov 22 2011 Time: 16:50:11
Then I try to run the c6accel_app and I get an error just after the "Tests for FFT functions succesful". The error I get is:
Assertion failed (ipsEventList [i].eventHandlerCount == 0). File : /home/elias/dvsdk_3_00_02_44/dsplink_1_61_03/packages/dsplink/gpp/src/../../gpp/src/ldrv/IPS/ips.c Line : 612
I have run the application again, having exported CE_DEBUG=2 and I attach the log file.5875.c6log.txt
What is the problem? Is the IFFT kernel corrupt?