This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

leopard board display and streaming stored file



hi all

i m trying to get output from videotest source my tv is connected with the board and it showing the logo of ridgerun but if i m running the video test source output is not coming in the tv

so whwre to see the output

>gst-launch videotestsrc ! TIDmaiVideoSink

this is the command for leo365

if in ubuntu im typing the command

>gst-launch videotestsrc ! ximageSink

a window is opening with colorful displsy

is this wht i shud xpect from dm365 test source also

and where to see the output

kailash